Skip to main content

Renesas Releases Next-Generation WPC Qi 1.3-Certified Reference Design for Automotive In-Cabin Wireless Charging

Provides ASIL B Functional Safety and Supports Fast Charging Modes for Latest Phone Models

March 15, 2022

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today released a next-generation customer reference design for automotive wireless charging stations. The new P9261-3C-CRBv2 provides industry-leading features that enable automotive manufacturers to quickly and efficiently deliver premium performance and safety features for in-cabin wireless charging.

The P9261-3C-CRBv2 solution includes the automotive-qualified wireless power controller P9261 with MP-A13 3-coils reference design as the wireless power transmitter (TX). It offers a large active charging area with high efficiency and exceptional EMC/EMI performance. The reference design offers compliance to the Wireless Power Consortium (WPC) Qi 1.3 standard EPP (Extended Power Profile) for 15W charging. It also supports proprietary charging profiles and is capable of 50W power delivery.

The new P9261-3C-CRBv2 design includes a Renesas RH850 automotive MCU as a host controller. This enables the system to provide functional safety features that comply with Automotive Safety Integrity Level B (ASIL B).

The P9261-3C-CRBv2 EVK can be controlled and monitored real-time by a graphical user interface (GUI). This GUI provides numerical readouts of key parameters, such as the selected coil, transmitter status, input voltage, buck output current, Tx power, and bridge voltage. The GUI enables easy programming changes and can update firmware. The GUI also supports tuning customer-specific variables related to hardware design, such as settings for foreign object detection (FOD).

“The P9261-3C-CRBv2 reference design demonstrates why automotive customers utilize Renesas’ easy-to-use design environment to swiftly develop next-generation solutions,” said Niall Lyne, Vice President, Automotive Power and Video Business Division at Renesas. “It offers the best wireless charging performance available and supports the latest safety features required by customers.”

P9261-3C-CRBv2 Reference Design Features

  • Complies with WPC Qi 1.3 standard for 15W charging
  • Supports proprietary charging profiles, capable of 50W fast charging
  • Functional safety with ASIL B compliance
  • Large active charging area
  • Best in class EMI performance, compliant to CISPR-25 standard
  • Easy-to-use GUI-based design software includes settings for Renesas’ patented Foreign Object Detection (QFOD)
  • Proprietary and Qi-compliant bi-directional Amplitude Shift Keying (ASK) and Frequency Shift Keying (FSK) communication

Wireless Charging Winning Combination

Renesas offers "Winning Combinations," compelling product combinations that help customers accelerate designs and get to market faster. The Automotive In-Cabin Wireless Power Solution Winning Combination includes the P9261, along with PMIC, power, and microcontroller offerings from Renesas. For more information on Renesas automotive Winning Combinations, go to Winning Combinations for Automotive | Renesas.

Availability

The new automotive wireless charging reference design, which includes the P9261-3C-CRBv2 EVK (Evaluation Kit), is available today. More information and a link to order the EVK can be accessed at: https://www.renesas.com/P9261-3C-CRBv2.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube and Instagram.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on