![Motor solution using the magnetic encoder](/sites/default/files/styles/banner_424x349/public/media/images/motor-solution-using-the-magnetic-encoder.jpg?itok=mCBVFt3m)
CPU Card for Motor Control
The CPU Card for Motor Control is an optional board for the Evaluation System for BLDC Motor. Using a CPU card and the evaluation system, users can easily evaluate...
The motor solution using a magnetic encoder is a solution to control motor by combining the permanent magnet synchronous motor (brushless DC motor) and the magnetic encoder. This solution enables to easily evaluate motor control using a magnetic encoder by using sample software in combination with the motor solution kit. Also, can easily check the functions, settings, and software processing of MCU for acquiring position information from the magnetic encoder.
A magnetic encoder is a kind of position sensor used for motor control or a sensor that converts the change in the magnetic field into an electric signal to output. The magnetic encoder has two types, The one outputs position information as an analog signal and the other outputs it as a digital signal like encoder. The magnetic encoder which outputs the digital signal can detect an angle using the timer function of the MCU like optical encoder. The magnetic encoder which outputs the analog signal, on the other hand, obtains the output signal (sin, cos) of sensor with the AD mounted on MCU and angle information with arc tangent.
Magnetic encoder outputting digital
Magnetic encoder outputting analog
Magnetic encoder outputting digital
Magnetic encoder outputting analog
The magnetic encoder which outputs the analog signal can obtain correct angle information by adjusting offset , gain (amplitude) and phase for the outputted analog signal. In this solution, these are automatically adjusted during startup, which enables to obtain correct angle information. If you use the magnetic encoder which outputs the digital signal, please refer to the sample software for vector control using encoder.
Offset・gain correction
Phase correction
In this solution, the operation has been confirmed using TMR magnetic encoder by TDK, TAD2141 (digital output) and TAS2143 (analog output).