Skip to main content

Renesas Introduces JEDEC-Compliant Precision Temperature Sensor for DDR5 Memory Modules

New IC Joins a Complete Family of DDR5 DIMM Solutions that Include the Registered Clock Driver, Power Management IC and SPD Hub

November 4, 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced a new precision temperature sensor, the TS5111, targeting DDR5 memory modules as well as a host of other applications such as solid-state disks (SSDs), computing motherboards, and communications equipment that require accurate, real-time temperature monitoring. The new JEDEC-compliant temperature sensor enables memory modules and other temperature-sensitive systems to run at peak efficiency and reliability with real-time, closed-loop thermal management algorithms.

The TS5111 plays a critical role in providing accurate, high-precision system temperatures with programmable warning flags that enable systems to exercise thermal control loop mechanisms such as memory refresh rates, fan speeds, and bandwidth throttling. Measuring a mere 0.8 x 1.3mm, the TS5111 is well suited for small form factor systems as well as applications such as memory and storage modules where proximity sensing is critical for reliable operation. The TS5111 supports I²C, SMBUS, as well as the new I3C Basic protocol for data rates up to 12.5 MHz and other advanced features like in-band interrupts, parity check, and packet error checks.

“We are proud to deliver the first JEDEC-compliant thermal sensor device for DDR5, which is currently in qualification with our key customers and ecosystem partners,” said Rami Sethi, Vice President, Data Center Business Division at Renesas. “The TS5111 has the potential to coalesce the entire computing industry around a single thermal sensor solution that supports the latest high-speed control bus interface and complies with an industry standard specification.”

The TS5111 joins a complete family of DDR5 solutions that enable companies to develop DDR5 DIMM solutions. The current Renesas DDR5 RDIMM ICs include the registered clock driver 5RCD0148HC1, power management IC P8900, and SPD Hub SPD5118.

Key Features of the TS5111 Temperature Sensor

  • Complies with the JEDEC JESD302-1 serial bus thermal sensor device specification
  • Temperature sensor accuracy
    • Typical 0.5 °C in 75 °C < TA < 95 °C range
    • Typical 1.0 °C in 40 °C < TA < 125 °C range
    • Typical 2.0 °C in -40 °C < TA < 125 °C range
  • Two-wire bus serial interface (I²C and I3C operation modes)
  • Up to 12.5 MHz transfer rate
  • 1.8 V & 1.1 V power supply input
  • Packet error check and parity error check functions
  • Bus reset function
  • Two unique addresses selected by SA pin
  • In band interrupt

Availability

The TS5111-Z1AHRI8 temperature sensor is available now in a 6-ball WLCSP package and is sampling to qualified customers. For additional information visit www.idt.com/TS5111.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on