TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced an inductive position sensor (IPS) technology for highly accurate motor position sensor ICs for robotics, industrial and medical applications. Utilizing non-contact coil sensors, the position sensing technology can replace expensive magnetic and optical encoders now commonly used in motor control systems that require absolute position sensing, high speed, accuracy and reliability.
The proprietary IPS technology from Renesas uses sensing elements consisting of copper coils etched on a printed circuit board (PCB) to detect the position of a metallic target. Unlike heavy magnet-based sensors, the IPS products can operate at 600 Krpm (electrical) and detect the position right at startup, while the propagation delay is less than 2μs, making them ideal for motors with high rotational speeds. Moreover, the sensor technology supports auto-calibration and linearization features, ensuring consistent performance throughout a motor’s operational life.
Based on the Vernier principle, the dual-coil sensor technology supports a resolution of up to 19 bits and an accuracy of up to 14 bits, which makes them superior to comparable products available in the market. The robust sensor technology will operate reliably in harsh environments, where they can be exposed to high temperatures, dust, moisture, vibration and electromagnetic interference (EMI). The induction sensors are immune to stray fields, require no maintenance, and are less susceptible to error than magnetic sensors. These advantages make induction position sensors a more attractive option than conventional optical encoders or magnetic-based encoders, which tend to be heavier and expensive.
“Our induction position sensor technology represents a significant leap forward in motor position sensors,” said Jan Leuckfeld, Senior Director, HPC Analog (Sensor) Division at Renesas. “They will enable us to provide differentiated motor position sensor ICs for industrial applications that are robust, highly accurate and cost-effective.”
“Position sensors for factory floors must endure extreme conditions such as humidity, high temperatures and vibration,” said Ulrich Marl, Key Account Manager at Lenord+Bauer, a Renesas customer and a leading manufacturer of encoders for industrial systems. “Through our collaboration with Renesas, we’ve integrated IPS-based technology into our encoder portfolio to ensure reliability and safety, while reducing downtime in critical applications.”
The induction position sensor technology will support commonly used UART, ABI and I2C communications interfaces, ensuring a seamless integration into industrial networks and facilitating real-time monitoring and data analysis. Additionally, the new sensor technology will be backed by a complete toolchain that includes dedicated software for user customization and precision optimization. Renesas plans to combine the new sensor with numerous compatible devices from its portfolio to offer a wide array of Winning Combinations. These Winning Combinations work together seamlessly to bring an optimized, low-risk design for faster time to market. More information about Winning Combinations are available at: renesas.com/win
Key Features of the New Sensor Based on IPS Technology
- Rotational speed: 600krpm (electrical)
- Resolution: up to 19 bits
- Accuracy: Up to 14 bits
- Digital interfaces: UART, ABI, I2C
- Extended ambient temperature range: -40 °C
- Two voltage supply ranges: 3.3V ±10% or 5.0V ±10%
- Over-voltage, reverse-polarity and short circuit protection: ±18V on both supply and output pins
- Adaptable to any full-scale angle range through coil design
Availability
Samples of the new induction position sensor are available in limited quantity today upon request. Please contact IPS@lm.renesas.com for more information or visit the Renesas website for technical details: https://www.renesas.com/products/sensor-products/position-sensors. Product names and specification details will be available in Q2/2024 when mass production begins.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. The leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube, and Instagram.
(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.