Skip to main content

Renesas Electronics Europe Releases Starter Kit Development Tools for RZ/A Family for High Performance and Low Cost Human Machine Interface Applications

November 4, 2020

Dusseldorf, November 12, 2013 — Renesas Electronics Europe, a premier supplier of advanced semiconductor solutions, today announced the availability of the Renesas Starter Kit for the RZ/A1 family of embedded processors. The RSK is the ideal starting point for design and creation of Human Machine Interface (HMI) applications and features everything needed for the development process. It has been specifically designed to reduce time to market and assist Renesas customers in creating rich HMI systems in the shortest time possible.

In 2013, Renesas launched the RZ/A1 device family featuring the world’s largest on chip SRAM of 10MB. It has been specially designed to meet the requirements of the graphical user interface developer, as it is able to drive screens up to XGA size without the need for external RAM. It is set to revolutionise the market, filling the gap in the market between the more traditional microcontroller and microprocessor solutions.

The Renesas Starter Kit, which is launched today, features a development board with the device itself as well as connectors for all the major supported communications peripherals on the device. These include CAN, Ethernet, camera interface, audio interface, SD card, USB 2.0 host and USB 2.0 function.

The kit is supplied with a 7-inch WVGA touch panel screen, so that systems designers can develop their own GUI directly on the development board.

In addition, it also includes all of the standard hardware features needed to start an evaluation or development, including a Segger JLINK-lite JTAG debugger, universal power supply and a PMOD debug screen to assist with application debugging.

From a software point of view, the kit is supported by both the ARM® IAR IDE and the ARM® DS-5 IDE. Additionally, the kit is supplied with a free GCC compiler, meaning that there are no additional costs from a software tools point of view to start programming. The kit also comes with over 15 different software examples, which include all source code demonstrating the capability of the device and form the basis of any developments customers may want to use.

There are four versions of the RSK available: a board only solution, options with and without the TFT screen, and with and without the debugger, ensuring that customers do not need to pay for tools that they do not require.

Ordercode Description RRP €
YR0K77210S000BE Renesas Starter Kit for RZ/A1, No debugger, No TFT 530
YR0K77210S001BE Renesas Starter Kit for RZ/A1, Including J-Link Lite debugger 580
YR0K77210S002BE Renesas Starter Kit for RZ/A1, Including TFT board 750
YR0K77210S003BE Renesas Starter Kit for RZ/A1, Including TFT board, J-Link Lite debugger 800

The tools are all orderable and shipping as of today.

(Remarks) ARM, Cortex and DS-5 are registered trademarks or trademarks of ARM Limited. Other product and service names that appear in this press release are trademarks or registered trademarks of their respective owners.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on