TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, has expanded its 32-bit microcontroller (MCU) offering with a new RX device for high-end industrial sensor systems. The latest addition, the RX23E-B, is a 32-bit device from its popular RX Family featuring a high-precision analog front end (AFE), specifically designed for systems that demand fast and accurate analog signal measurements.
The new MCU integrates a 24-bit Delta-Sigma A/D converter capable of achieving a conversion speed of up to 125 kSPS (125,000 samples/second) -- eight times faster than the existing RX23E-A. It can process accurate A/D conversion while reducing RMS noise to 1/3 (0.18µVrms @1kSPS) when compared to the RX23E-A. The RX23E-B facilitates faster and more precise measurements of critical parameters such as strain, temperature, pressure, flow rate, current and voltage, making it ideal for high-end sensor devices, measuring instruments, and test equipment. In particular, the RX23E-B offers sufficient performance to drive force sensors used in industrial robots, which often demand measurements as fast as 10 µsec (100,000 samples/second). The MCU also reduces overall system size and the component count by incorporating the AFE and the MCU on a single chip.
“With the addition of the RX23E-B which comes with an AFE sensor interface, we can now serve a broad range of sensing applications from mid- to high-end systems,” said Sakae Ito, Vice President of the IoT Platform Business Division at Renesas. “We will continue to extend our product options to meet the growing needs of battery-powered and wireless sensors that demand low power consumption.”
"At Meiko Electronics, we have been developing evaluation boards and providing design support to our customers since the RX23E-A product was introduced,” said Takatsugu Nemoto, President at Meiko Electronics. “Now, with the introduction of the RX23E-B with a high-speed delta-sigma A/D converter, we anticipate many customers will be able to experience the benefits of its enhanced conversion performance, compact board design and reduced component count."
Similar to the RX23E-A, the RX23E-B incorporates a 32-MHz RXv2-based CPU with digital signal processing (DSP) instructions and a floating point unit (FPU), and combines the AFE into a single chip using the same fabrication process. It offers new peripheral functions such as a 16-bit D/A converter, which enables measurement adjustments, self-diagnosis, and analog signal output. The device’s +/-10V analog input enables +/-10V measurement with a 5V power supply without requiring external components or additional power supply. An LCD controller with a maximum of 40 SEG x 4 COM and a real-time clock (RTC) function are also included.
In large-scale instruments that need to control and take measurements of multiple targets such as robot arms, gas and liquid analyzers, there has been a significant demand for distributed processing architecture. In distributed processing design, instead of relying on a dedicated MCU to manage all functions, each function can operate as a separate module, responsible for tasks such as motor control, sensor measurement and temperature control. This modular approach allows for independent development, offers greater design flexibility and simplifies maintenance. As each module needs an MCU for calculations, engineers can develop sensor modules more easily using an MCU with a built-in AFE, than combining a discrete AFE chip and a separate MCU.
The RX23E-B offers a version that supports an A/D conversion data rate of up to 125 kSPS, and a version that supports up to 31.25 kSPS. Both products offer flexible data rate settings ranging from 3.8 SPS to the maximum value, allowing users to choose the best balance between data rate and noise for their specific system requirements. The products are available in a 5.5 mm square 100-pin BGA package and a 6 mm square 40-pin QFN package for compact applications, as well as wide pin packages ranging from 48- to 100-pin options.
Winning Combinations
Renesas has combined the new RX23E-B MCU, designed for precise pressure measurement and control, with intelligent power devices tasked with driving solenoid valves, to develop the high-speed Pressure Control Solution. The integrated high-precision AFE provides precise pressure control and minimizes the component count for the design which reduces the BOM costs and board mounting area. These Winning Combinations are technically vetted system architectures from mutually compatible devices that work together seamlessly to bring an optimized, low-risk design for faster time to market. Renesas offers more than 400 Winning Combinations with a wide range of products from the Renesas portfolio to enable customers to speed up the design process and bring their products to market more quickly. More information can be found at renesas.com/win.
Availability
The RX23E-B is available now, along with a Renesas Solution Starter Kit for RX23E-B. Using this kit, engineers can evaluate the operation and functionality of the AFE and signal conversion without the need for software development. More information about the RX23E-B and the starter kit is available at www.renesas.com/rx23e-b.
Renesas MCU Leadership
The world leader in MCUs, Renesas ships more than 3.5 billion units per year, with approximately 50% of shipments serving the automotive industry, and the remainder supporting industrial and Internet of Things applications as well as data center and communications infrastructure. Renesas has the broadest portfolio of 8-, 16- and 32-bit devices, delivering unmatched quality and efficiency with exceptional performance. As a trusted supplier, Renesas has decades of experience designing smart, secure MCUs, backed by a dual-source production model, the industry’s most advanced MCU process technology and a vast network of more than 200 ecosystem partners. For more information about Renesas MCUs, visit www.renesas.com/MCUs.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. The leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.
(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.