Flammable Gas Leakage Detector Reference Design
The AS043-FGSLEAKPOC2Z Flammable Gas Leakage Detector is a battery-operated, standalone system with wireless connectivity using low-power Wi-Fi communication. This...
This is a battery-operated stand-alone system with wireless connectivity that uses low-power Wi-Fi communication to detect the leakage of flammable gas. It can be a very useful system for industrial and household applications. In this system, the information about the Liquefied Petroleum Gas (LPG)/Piped Natural Gas (PNG) gas leakage can be detected, alarmed and communicated to users through a single microcontroller (MCU) with built-in Wi-Fi communication. The Wi-Fi communicates with the nearest router and sends the updates via push notification over the user's phone through a dedicated mobile app.
System Benefits:
Available on Lab on the Cloud - Use our PC-based GUI to instantly start configuring and testing.
Launch Lab on the Cloud