Overview
Description
Release Information
Region | Model No. | Shipment after modification of the Safety Standard IEC 62368-1 *Important 2 |
---|---|---|
Japan | QB-COMMON-PW-JP | no change |
America | QB-COMMON-PW-EA | no change |
Europe | Bundled with the IECUBE and PG-FG5 (not separated) |
no change |
China | QB-COMMON-PW-CN | Discontinued |
Hong Kong | QB-COMMON-PW-HK | Discontinued |
Korea | QB-COMMON-PW-KR | To be handled after individual discussion |
Singapore | QB-COMMON-PW-SG | Discontinued |
Taiwan | QB-COMMON-PW-TW | Shipping deadline: February 7, 2025 |
Important :
- The power supply adapter is shipped only for orders from the destination area. For model numbers in other regions than above, contact one of the Renesas Electronics distributors or sales representatives in your area.
- In response to modification of the Safety Standard IEC62368-1, we will discontinue our production of these power adapters "QB-COMMON-PW-xx" for the IECUBE and PG-FP5 (Discontinued product) which are intended to use in Asia excluding Japan.
For Taiwan, shipment is not allowed after the qualification deadline (February 7, 2025), please inform us of the final required quantity through your local Renesas Electronics sales office or distributor before the deadline. No deadline is set for Korea, however, each order will be handled after individual discussion. We will also stop shipment of the IECUBE to Asia because there are no replacements for these power adapters.
We will continue shipment to Japan, U.S., and Europe as we have done till now.