Skip to main content

Adesto Announces Availability of Industry’s First Truly Open Edge Server for Building Automation and Industrial IoT

April 22, 2019

SANTA CLARA, CA – Adesto® Technologies Corporation (NASDAQ: IOTS), a leading provider of innovative application-specific semiconductors and embedded systems for the IoT era, announced general availability of its next-generation edge server for building automation and industrial IoT applications. SmartServer™ IoT is the industry’s first truly open, full-featured and end-to-end industrial-rated IoT edge server. Its out-of-the-box device management services, intuitive user interface and programmable interfaces and applications enable system integrators to deploy solutions in an afternoon, and OEMs to create custom applications with ease.

Smart buildings represent a rapidly growing segment of the Industrial IoT market as facility managers increasingly see the benefits of merging traditional building automation and control (BAC) systems with emerging sensing, communications and cloud technologies. With Adesto’s SmartServer IoT, customers can meet today’s challenge of creating truly smart buildings by integrating their systems’ multitude of non-interoperable communications protocols – which have evolved over the years to support each buildings’ diverse functions, such as lighting, security, HVAC, fire detection and others – with new sensing, analytics and predictive AI services not available through BAC systems.

“Edge servers represent the crossroads where traditional operational systems meet the IoT, and today they are needed across just about every industrial and built-in environment,” said Adarsh Krishnan, principal analyst, ABI Research. “Edge servers are not all created equal, however. Bridging the separate islands of automation in buildings without losing the considerable investment in each specialized control network is key. This path to more effective building automation solutions is what Adesto is addressing today with SmartServer IoT.”

SmartServer IoT supports multiple protocols and applications, enabling the convergence of diverse systems into a single edge networking and compute platform. It features built-in support for popular building automation protocols and services; open northbound interfaces to any remote client, workstation or web application; open southbound interfaces; and a data abstraction layer for connecting with emerging IoT protocols and devices. With SmartServer IoT, businesses can embrace their existing, perfectly functional control and management systems, and enhance them by securely connecting them to advanced IoT technologies.

“By supporting both BAC work flows and IoT applications and providing an open ecosystem, Adesto’s SmartServer IoT eliminates the painstaking task of integration that is the industry norm when implementing IoT projects in commercial buildings,” said Tim Hopkins, COO, Envigilant Systems, an Allied Telesis Division. “While a typical integration project can take months, we were able to get going with SmartServer IoT in a matter of hours. SmartServer IoT gives us the ability to not only reduce integration frictions, but also create our own services for data and controls. We’re excited to pass this benefit on to our customers by enabling them to maximize their ROI and enhance the building experience for owners and occupants.”

“Traditional building and industrial control systems aren’t going away,” said Apurba Pradhan, vice president of marketing, Embedded Systems Division, Adesto. “Rip and replace is just not an option for building or operations managers with existing automation infrastructure based on BACnet, LON, Modbus or other field bus systems that were very costly to put in place. With SmartServer IoT, we leverage our 30 years of expertise in industrial communications and networking to simplify the deployment of advanced IoT applications in such market verticals for web developers and system integrators.”

A Look Inside SmartServer IoT

The SmartServer IoT provides multi-protocol IoT gateway functionality with edge compute resources and APIs to optimize industrial IoT workflow between the cloud and edge for industries such as building automation, transportation and industrial controls. Key enablers include:

  • An end-to-end IoT solution, with modular interfaces for leading industrial communications protocols and IP network and data abstraction layer, eliminating the requirement to integrate protocol stacks and abstract the data from a variety of device types
  • Secure IoT messaging to remote clients and cloud services to gather data from devices efficiently from any public or private cloud without opening unsecure ports or punching holes through firewalls
  • Edge services for controls and automation, with pre-integrated device and data management apps—such as connecting, routing, scheduling, data logging and alarming—all operating at the network edge for faster, more responsive systems
  • User-friendly web-based management system for simplifying the integrator workflow of creating, provisioning and managing devices with configurable dashboards, alarms and reports
  • An extensible, open integration platform based on Linux, with freely available modern RESTful APIs for accelerating web apps and HTML development, and MQTT for custom controls applications; all ensuring integration with any IoT device or application

Availability

SmartServer IoT is available now. For more information including pricing on pilot and commercial opportunities visit https://www.dialog-semiconductor.com/products/systems-and-software/smartserver-iot.

About Adesto Technologies Corporation

Adesto Technologies Corporation (NASDAQ:IOTS) is a leading provider of innovative application-specific semiconductors and embedded systems for the IoT era. The company’s technology is used by more than 2,000 customers worldwide who are creating differentiated solutions across industrial, consumer, medical and communications markets. With its growing portfolio of high-value technologies, Adesto is helping its customers usher in the era of the Internet of Things.

Adesto, the Adesto logo, and SmartServer are trademarks or registered trademarks of Adesto Technologies Corporation or its subsidiaries in the United States and other countries. Other company, product and service names may be trademarks or service marks of others.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on