Skip to main content

IDT Improves RF Switch Performance with New SPDT Switch Featuring KZ Constant Impedance Technology

IDT’s F2923 Provides Constant Impedance on All Ports During Switching Transitions without Compromising Isolation, Linearity or Insertion Loss

December 1, 2015

SAN JOSE, Calif., Nov. 24, 2015--Integrated Device Technology, Inc.® (IDT®) (NASDAQ: IDTI) today introduced the industry’s first single-pole, double-throw (SPDT) RF switch featuring its patent-pending KZ constant impedance technology. The IDT F2923 is a low insertion loss SPDT absorptive RF switch designed for a multitude of RF applications, including base stations (2G, 3G, 4G, 5G), wireless backhaul, CATV, and portable handhelds.

The KZ feature controls all port impedances when switching between RF ports, preserving the return loss. Standard switches without KZ create a large voltage standing wave ratio (VSWR) transient when switching RF paths because the impedance of the switch is not well controlled during the switching event. A VSWR transient can degrade system performance and reduce reliability.  Benefits of Kz in different dynamic or “hot switching” scenarios include:

  • Minimizing switched Tx/Rx Synthesizer pulling and recovery time in TDD systems
  • Avoiding damage and error-inducing transients when switching between two RF elements such as PAs, drivers and LNAs.
  • Minimizing transient amplitude and phase error on the unswitched path(s) when switching a path of a distribution network such as a 3 dB coupler or 4 way splitter

 “With this latest SPDT switch, we highlight our new KZ technology to dramatically improve hot-switching performance,” said Chris Stephens, general manager of IDT’s RF division. “The F2923 demonstrates yet again IDT’s leadership in the core RF innovations that system developers desire.”

In addition to KZ technology, the device delivers:

  • Insertion loss of only 0.48dB at 2GHz
  • IIP3 greater than 66dBm @ 2GHz
  • Industry-leading isolation of 74 dB at 2 GHz

 Covering a broad frequency range from 300kHz to 8000MHz, IDT’s innovative Kz technology ensures the device delivers near-constant impedance (VSWR < 1.4:1 compared to 9:1 for standard switches) when switching from one RF port to another while not compromising isolation, linearity, or insertion loss. The F2923 uses a single positive supply voltage of 3.3V and supports standard 1.8V and 3.3V control logic levels.

Availability

            The F2923 switch is sampling and comes in a 4 x 4 mm 20-TQFN package.

About IDT RF Products

IDT offers high-performance and full-featured radio frequency (RF) products that deliver exceptional performance in compact packages. All IDT RF signal path devices are silicon based, offering inherent advantages over GaAs-based products. The portfolio includes RF mixers, RF and IF variable gain amplifiers (VGA), digital step attenuators (DSA), demodulators, broadband modulators, RF switches, and wideband voltage variable attenuators. IDT’s RF devices are ideal for use in such products as cellular 4G base stations, broadband repeaters, distributed antenna systems and microwave backhaul equipment.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on