Skip to main content

IDT Launches Industry’s Highest Efficiency 15 W Wireless Power Transmitter and Receiver Solution

Supporting the Wireless Power Consortium’s Qi Standard, the Chips Enable Wireless Charging in New Categories of Consumer Products and Infrastructure

February 27, 2016

SAN JOSE, Calif., Feb. 22, 2016— Integrated Device Technology, Inc.® (IDT®) (NASDAQ: IDTI) today introduced two new devices that deliver a complete high-efficiency wireless charging solution for electronics demanding up to 15 W of output power . Supporting wireless charging for new categories of consumer products and infrastructure, the highly integrated chips deliver industry-leading power conversion efficiency of over 86 percent from transmitter input to receiver output, reducing system losses and improving thermal performance while rivaling traditional wired power conversion architectures.

Compatible with the Wireless Power Consortium (WPC) Qi standard, the new transmitter and receiver further enhance IDT’s leadership position in wireless power, where the company’s 5 W and 3W solutions are already deployed into high-volume smartphones and wearables.  

The new P9240A transmitter is ideal for standalone transmitter pads and embedded furniture, as well as infrastructure applications in airports, hotels and cafes. The companion P9220 receiver is designed for products that require high current charging like tablets and phablets, mini PCs, medical instruments and wireless speakers, as well as “fast charging” smartphones. Both transmitter and receiver ICs deploy a high performance microprocessor for maximum flexibility and performance optimization.

“IDT has led the way in wireless power, having shipped more than 70 million of our chips for leading-edge consumer products,” said Dave Shepard, vice president and general manager of IDT’s Consumer Products Division. “By introducing these new highly integrated, higher power, energy-efficient devices, we are bringing our expertise and experience to new application groups so they, too, can enjoy the benefits of wireless charging.”

The P9240A transmitter accepts a wide range input (4.25-21V) and features proprietary slew rate control for optimal EMI performance and low power standby. The flexible P9240A core provides power level scalability and performance optimization. The P9220 receiver is highly integrated, with an active internal rectifier and output LDO with support for all mainstream communication interface protocols. Similar to the P9240A transmitter, the P9220 receiver’s core maximizes flexibility and customization.  

Pricing and Availability

The P9240A is available in a 40-QFN5X5 package and is priced at $3.75 each for a 10k lot. The P9220 is available in a WLCSP package and is priced at $2.50 each for a 10k lot.

About IDT Wireless Power

          IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC) and AirFuel Alliance as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA (now AirFuel Alliance) standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers' applications. IDT's market-leading products in timing, wireless power transfer, serial switching and interfaces are among the company's broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol "IDTI." Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

###

© 2016, IDT. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., or its wholly-owned subsidiaries around the world. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on