Skip to main content

IDT Makes Wireless Power Accessible to the Mass Market

Eliminating Traditional Barriers, IDT’s New Plug-and-Play Reference Kits Enable Engineers to Integrate Wireless Charging into Product Designs in a Matter of Hours

August 25, 2015

SAN JOSE, Calif., Aug. 25, 2015 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), today introduced groundbreaking turnkey wireless power kits that make integrating wireless charging easy, affordable and practical for a broad range of consumer electronics. The new Qi-compliant transmitter and receiver reference kits deliver plug-and-play ease of integration, enabling engineers to incorporate wireless charging capabilities into their designs in a matter of hours.

“Integrating wireless power capabilities into existing electronics is a complex process, and one of the factors that has unquestionably slowed its adoption throughout the electronics industry,” said David Green, research manager, Power Supplies & Wireless Power at IHS. “This approach of providing self-contained, ready-to-go wireless charging kits has the potential to change the landscape for those not yet equipped.”

The 5-Watt, 5-Volt solution is suitable for a wide range of applications, including PC peripherals, furniture, medical devices, and other portable devices still hindered by traditional contact-based charging bases or cables.

“There is heavy demand for wireless power in mid- and low-volume applications that is currently underserved in the market,” said Greg Waters, president and CEO at IDT. “By offering a pre-configured, comprehensive, out-of-the-box solution, we make it possible for customers to design a wireless power solution with very little to no engineering support required. This results in a quick-turn and highly-scalable model that enables customers to take full advantage of IDT’s industry-leading wireless power products.”

The transmitter and receiver reference kits are built around proven IDT wireless power semiconductors, and include easy-to-use reference boards and comprehensive design support collateral. Support materials include instructional videos, user manuals, foreign object detection (FOD) tuning guides, layout guides, layout instantiation modules, schematics, bill-of-materials (BOM), Gerber files, and more.

Both reference kits offer 2-layer board layout files, providing maximum flexibility for most applications. The boards are Qi-compliant for use as-is.

The kits can be used for immediate prototyping. An associated layout module enables direct instantiation on to a system board, while an optimized and fully tested BOM takes the guess-work out of component selection. Foreign object detection (FOD) tuning is supported via selectable pre-programmed curve settings and extensive collateral documenting FOD tuning for these devices.

“Digi-Key anticipates great interest in these industry-first wireless power products, and we’re able to offer kits purchased through digikey.com’s wireless charging landing page at less than half the price of traditional evaluation kits of this type,” said David Stein, vice president, Global Semiconductor at Digi-Key Electronics. “With next-day delivery, engineers can go from concept to prototype in fewer than 24 hours. In addition, the full bill-of-materials and pre-production samples can be ordered with just a few clicks, making it easy to place production orders when the time is right.”

Pricing and Availability

The P9038-R-EVK and P9025AC-R-EVK are available now at suggested retail prices of $40 and $30, respectively, and can be ordered directly from participating distribution partners. For the best prototyping and evaluation experience, it is recommended to order both the transmitter and receiver kits. Limited quantities are available and will be sold on a first-come, first-served basis. Free samples are available for approved customers.

See the un-boxing and start-up video here.
To learn more, visit www.idt.com/go/WPkits

About IDT Wireless Power

IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

About IDT

Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on