SAN JOSE, Calif., September 14, 2017 – Integrated Device Technology, Inc. (IDT) (NASDAQ: IDTI) today announced a live demonstration of its latest 200G VCSEL and DML Drivers, and TIA ICs at ECOC 2017. This newest family of 2- and 4-channel PAM4 CDR/Retimers, 1x and 4x VCSEL and DML Drivers, and TIAs will help address current datacenter challenges, enabling IDT’s customers to upgrade hyper-scale datacenter and cloud computing infrastructure from 100G to 200G and beyond.
In recent years, hyper-scale datacenters have pushed the boundaries of network design to support the highly virtualized and scaled-out applications of the modern age. As cloud and networking services become increasingly central to consumers’ lives, IDT’s latest solutions help datacenter operators to meet the continuously growing demands for higher densities and greater speeds brought on by the overwhelming increase in data traffic. It is essential that they are able to quickly and easily transition to higher data rates as needed in order to meet business requirements.
“Datacenters are facing enormous pressure to keep the pace, supporting the higher bandwidths required to deliver an exceptional experience for their customers. IDT’s latest family of 50G/200G, PAM4 CDR/Retimers, VCSEL and DML Drivers and TIAs will make it possible for datacenter operators to upgrade their servers from 100G to 200G and beyond, delivering the data rates necessary for emerging applications – such as live video streaming, AI chatbots, augmented and virtual reality – that demand a new level of performance from cloud infrastructure,” said Dr. Raluca Dinu, VP/GM of the Optical Interconnect Division at IDT, Inc. “We are very excited to be the first company to begin sampling 2- and 4-channel analog 200G PAM4 Clock Data Recover/Retimers based on advanced CMOS technology to our customers.”
IDT’s Short and Long Reach Configurations
Application Distance |
SR Configuration(s) |
Long Reach Configurations |
SFP28+ |
HXT44100: 1ch – 28Gbps VCSEL Driver HXR44100: 1ch – 28Gbps TIA+PA Receiver |
HXT44100: 1ch – 28Gbps DML Driver HXT44101: 1ch – 28Gbps DML Driver, packaged HXR44100: 1ch – 28Gbps TIA+PA LR Receiver |
HXC44200: 2ch – Bi-directional 28Gbps CDR / Retimer |
||
QSFP28+ |
HXT44400: 4ch – 28Gbps VCSEL Driver HXR44400: 4ch – 28Gbps TIA+PA Receiver |
HXT44400: 4ch – 28Gbps DML Driver HXT44401: 4ch – 28Gbps DML Driver, packaged HXR44400: 4ch – 28Gbps TIA+PA LR Receiver |
HXC44400: 4ch – 28Gbps CDR / Retimer |
To see our live demonstration, please visit IDT at ECOC 2017, stand 417, September 18-20 in Gothenburg, Sweden. To schedule a meeting with IDT executives at the show, please contact [email protected].
About IDT
Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT can be found at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
© 2017, Integrated Device Technology, Inc. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.