Skip to main content

IDT Teams with Samsung to Integrate Wireless Charging

IDT Wireless Power Technology Now Used Across a Broad Range of Samsung Products 

October 19, 2015

SAN JOSE, Calif., Oct. 19, 2015-- Integrated Device Technology, Inc. ® (IDT®) (NASDAQ: IDTI) today announced that IDT teamed with Samsung to deliver wireless charging for its Galaxy S6 edge+ and Galaxy Note5 smartphones, wireless charger, and Samsung Gear S2 smartwatch charging pad. The highly flexible IDT technology includes all of the semiconductor hardware and associated software required to support mobile devices to be charged without a wired connection. IDT also joined with Samsung for the Galaxy S6 wireless charger.

“We have worked closely with Samsung to ensure the company’s latest consumer products deliver the high-quality wireless charging experiences consumers are coming to expect,” said Mario Montana, IDT vice president and chief sales officer. “Among their many other noteworthy features, Galaxy S6 edge+, Galaxy Note5 and Gear S2 now boast the latest in wireless power technology for ease of use and convenience.”

The latest IDT ICs used in Samsung products are highly programmable with built-in microprocessor cores, supporting Samsung’s customization of its own unique features such as fast charge, first on Galaxy S6 edge+ and Galaxy Note5, coupled with Samsung’s wireless charger. This feature enables users to charge the Galaxy S6 edge+ or Galaxy Note5 device up to about 1.5X faster than legacy wireless charging solutions.

In addition to providing wireless power technology to global leaders like Samsung, IDT recently introduced wireless power kits that enable electronics companies of any size to easily integrate wireless charging capabilities into their product design, like the compact Samsung Gear S2 charging pad.

About IDT Wireless Power

IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners. FAST CHARGE™ is the trademark of Samsung

Available Translations

Share this news on