Skip to main content

Intersil Ships Automotive Industry's First Full HD LCD Video Processor

Highly integrated TW8844 instantly displays rearview camera live video, exceeding industry standard by 4x to prevent backover accidents

July 10, 2017

MILPITAS, Calif., July 10, 2017 /PRNewswire/ --Intersil, a subsidiary of Renesas Electronics Corporation (TSE: 6723), today announced the TW8844 LCD video processor that interfaces with the latest generation of automotive SoCs. The highly integrated TW8844 is the first high-definition (HD) 1080p LCD video processor with analog video decoder, two scalers and MIPI-CSI2 SoC interface, and builds on Intersil's automotive video leadership in infotainment and display systems. The TW8844 provides the reliability automakers require to ensure their rearview camera systems are compliant with the U.S. Federal Motor Vehicle Safety Standard (FMVSS-111) for preventing injury or death caused by backover accidents. The TW8844 enables the migration from analog to digital camera systems, and supports a variety of video interfaces and LCD panel resolutions up to full HD 1920 x 1080. The TW8844 LCD video processor is ideal for center stack/head units, full display rearview mirrors, instrument cluster displays, and dual headrest rear-seat entertainment systems. Watch a video on the TW8844 solution.

Automakers are starting to make rearview camera systems standard equipment for all new car models worldwide. In the U.S., the National Highway Traffic Safety Administration mandated in March 2014 that automakers implement "rear visibility technology" as standard equipment for all vehicles under 10,000 pounds, as part of the Kids Transportation Safety Act. The new FMVSS-111 regulation specifies that the area behind a vehicle must be visible to the driver when the vehicle is placed into reverse, thereby minimizing blind spots. The law aims to reduce the number of deaths and injuries caused by driver backup accidents, many involving young children. The FMVSS-111 law requires that all new vehicles sold in the U.S., beginning in May 2018, have rearview backup cameras and the rear camera video must display in less than two seconds after the driver places the vehicle into reverse gear.

The TW8844 video processor with MIPI-CSI2 output and TW8845 video processor with BT.656 output exceed the requirements of the FMVSS-111 law, displaying live video with graphics overlay in less than 0.5 seconds after vehicle ignition. The TW884x provides a robust rear-camera architecture to overcome the fast boot reliability issues inherent with today's more complex center-stack systems. Today's head units are prone to operating system (OS) software freezes and hang-ups that display a frozen image or prevent the rear camera from displaying live video. With SoCs running increasingly complex operating systems, software freezes and hang-ups are more common. The TW884x eliminates this problem by monitoring the SoC and camera output to determine if they are in a frozen or corrupted state. If the TW884x detects any issue, it bypasses the SoC and instantly displays the rearview camera video.

"The TW884x's frozen detection feature is hardwired to trigger an interrupt signal if thresholds are violated, ensuring the vehicle's rearview camera is FMVSS-111 compliant and live video is instantly displayed," said Philip Chesley, senior vice president of Precision Products at Intersil. "In addition, the TW884x's rearview camera bypass architecture decouples the camera-to-display signal path from the rest of the infotainment system, which makes attaining an ISO 26262 functional safety rating on the camera system easier for automakers."

  • Support several video inputs from analog or digital HD cameras:
    • 10-bit ADC NTSC/PAL analog video decoder supports differential, pseudo differential, and single ended composite video inputs (two differential or four single-ended), with built-in short-to-battery and short-to-ground diagnostics
    • Two independent digital RGB input ports up to 24-bit RGB at 160MHz (1080p) each
    • Two LVDS OpenLDI input ports (shares pins with the 2nd DRGB input) in 1-ch or 2-ch input mode, with 100MHz (max) per channel in 1-ch mode or 160MHz in 2-ch mode
    • Support either one full HD input (1080p) or two HD inputs (720p)
  • Provide system flexibility to drive most LCD panels:
    • LCD path for TTL/TCON up to 24-bit DRGB, 160MHz (max)
    • LVDS OpenLDI: dual channel, 100MHz (max) per channel in 1-ch mode or 160MHz in 2-ch mode
    • TW8844 supports 4-lane MIPI-CSI2 output for up to 1080p, with up to 1Gb/lane
    • TW8845 supports BT.656 output to the SoC with resolutions up to 720p
       
  • Two input measurement engines with frozen/abnormal image detection diagnostics to monitor input from the SoC and camera
  • EEPROM fast boot allows register programming without need for external microcontroller
  • Two separate H/V scalers for outputting up to 1080p (1920 x 1080) resolution, allow processing of two different sources simultaneously, while outputting different data to the SoC and display, or they can simultaneously drive two different displays with different content
  • Automatic Contrast Adjustment (ACA), white balance and gamma correction optimizes video quality
  • Smooth input switching allows switching between various input sources without screen flicker
  • AEC-Q100 Grade-2 qualified for operation from -40°C to +105°C

The TW8844 and TW8845 can be combined with Renesas'  R-Car SoC family, as well as the  ISL78302 dual LDO,  ISL78322 dual 2A/1.7A synchronous buck regulator, and  ISL78228 dual 800mA synchronous buck regulator to provide power rails for the TW884x, SoC and other key components on the automotive infotainment system board.

The TW8844 video processor with MIPI-CSI2 output is available now in a 14mm x 20mm, 156-lead LQFP package, and is priced at $10.00 USD in 1k quantities. For more information on the TW8844 and evaluation board, please visit: www.intersil.com/products/tw8844.

The TW8845 video processor with BT.656 output is available now in a 14mm x 20mm, 156-lead LQFP package, and is priced at $9.50 USD in 1k quantities. For more information on the TW8845 and evaluation board, please visit: www.intersil.com/products/tw8845.

 

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil, a Renesas Company. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on