MILPITAS, CA -- (MARKETWIRE) -- 03/14/13 -- Intersil Corporation (NASDAQ: ISIL), a leader in the design and manufacture of high-performance analog, mixed-signal and power management semiconductors, will introduce its latest PowerNavigator™ digital design system at this year's APEC in Long Beach March 17-21, booth 619.
The PowerNavigator GUI offers a single software platform for all PMBus-enabled Power Management products at Intersil, meeting all user requirements with complete design editing from design start to hardware implementation.
The PowerNavigator software allows simple configuration and monitoring of multiple PMBus-based products using a PC with a USB interface. The new PowerNavigator's intuitive graphical user interface, with power centric-intelligence, saves days of design time compared with other analog-based designs. It can monitor large systems through dashboard views, allows for easy debugging during prototyping, and provides comprehensive visualizations and power-centric intelligence such as sequencing and fault management.
Configuration and setup of the entire power system using Intersil PMBus products lets designers architect their systems at the beginning of a project before hardware is committed, saving time and cost. System-level project files allow the entire power system to be configured simultaneously eliminating the need for multiple files, enabling collaborative sharing and debugging across multiple locations and a seamless transition to the production environment.
For more information on PowerNavigator visit: http://www.intersil.com/en/products/power-management/zilker-labs-digital-power/powernavigator.html
Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.