Skip to main content

New VersaClock 6 Programmable Clock Generators Achieve Best Performance to Date for IDT’s Award-Winning VersaClock Family

 Sub-500 Femtosecond Phase Jitter Performance, Combined with Low Operating Power, Opens Up a New Class of Programmable Timing Products for High-Performance Applications

October 14, 2015

SAN JOSE, Calif., Oct. 7, 2015-- Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today introduced the VersaClock® 6 programmable clock generator family to deliver flexible, low-power timing for demanding high-performance applications. With RMS phase jitter of less than 500 femtoseconds (fsec), the VersaClock 6 products deliver the best performance to date for IDT’s award-winning VersaClock family, offering an exceptional combination of jitter performance, flexibility, and low operating power.

With RMS phase jitter less than 500 fsec over the full 12 kHz to 20 MHz integration range, the new devices meet the stringent jitter and phase noise requirements of applications and standards such as 10G Ethernet, enterprise storage SAS and SATA, PCI Express Gen 1/2/3, XAUI, SRIO, stringent PHY reference clocks and the newest generations of high-end FPGAs — all while operating at about half the core power of competing devices. The devices’ core current consumption of 30 mA eases system thermal constraints and reduces operating power expenses. In addition, the VersaClock 6 devices are footprint compatible with their VersaClock 5 counterparts, enabling performance scalability with minimal design changes.

“These latest VersaClock products offer unmatched power savings for a programmable clock generator with this level of performance,” said Kris Rausch, general manager of IDT’s multi-market timing division. “The VersaClock 6 devices enable customers to meet their systems’ stringent jitter and low power requirements while at the same time reducing board space and bill of materials costs. With its winning combination of low phase jitter and power consumption, the VersaClock 6 device is ideal for such markets as high-end consumer, networking, computing, industrial and communications.”

The VersaClock 6 programmable clock generator offers universal output pairs that are independently configurable as LVDS, LVPECL, HCSL, or dual LVCMOS and can generate any output frequency from 1 MHz to 350 MHz on each output pair independently. The new devices are the:

The VersaClock 6 flexibility enables customers to get the exact functionality they need in a cost-effective manner, while exceptional RMS phase jitter performance addresses the requirements of high-performance applications and phase noise performance meets the latest FPGA specifications.

The 4 mm x 4 mm 24-VFQFPN package is footprint compatible with VersaClock 5 devices, enabling performance scalability with minimal design change.

See the VersaClock 6 introduction video on IDT’s YouTube channel.

Pricing and Availability

The VersaClock 6 family devices are available now with the 1K price of $5.20 for the 5P49V6901, $4 for the 5P49V6914 and $3.20 for the 5P49V6913.

About IDT Clock and Timing Solutions

With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. For more information about IDT’s leading portfolio of timing products, please visit http://www.idt.com/go/timing.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

 

###

 

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

 

 

Share this news on