Optimized for Emerging Markets Offering a Perfect Blend of System Integration and Performance
TOKYO, Japan, August 25, 2011 — Renesas Electronics Corporation (TSE: 6723) and its subsidiary, Renesas Mobile Corporation, today announced a new member of the R-Car series of automotive systems-on-chip (SoCs), the R-Car E1, offering low power consumption and high system integration targeting the cost-sensitive market of car navigation and multimedia systems including high-end car radios.
With the R-Car E1 SoC, Renesas strengthens its position in entry navigation systems, as this device offers a perfect balance between system integration and cost. The R-Car E1 device is powered with a single ARM®Cortex™-A9 32-bit RISC CPU core (enhanced with the NEON™ extension) running at 533 megahertz (MHz), which achieves a maximum processing power of 1,330 Dhrystone million instructions per second (DMIPS). The Graphics Processor Unit (GPU) is Imagination Technologies' PowerVR™ SGX531 and processes up to 14M triangles/s and is capable of delivering up to 1.4 gigaflops for accelerated graphics.
To help customers minimize board space and costs of their navigation solutions, targeting emerging markets and cost-sensitive applications, the R-Car E1 SoC has a balanced selection of integrated peripherals and functions. With multiple channels of 10-bit A/D converters, customers can simplify the interface to gyroscopes and accelerometers. The R-Car E1 SoCs also offers CD-ROM hardware-decoding capabilities and media interfaces for digital formats such as SD and USB.
Two output displays are supported—one output display is a digital RGB interface targeted for the main screen, while the second is an analog output supporting PAL/NTSC formats, enabling cost-effective, rear-seat entertainment. The integrated digital-camera interface facilitates the integration of a backup-camera or external video content. The R-Car E1 video processing unit (VPU) is capable of decoding up to 720p HD video codecs.
Equipped with various standard and automotive communication interfaces (CAN, MOST, Ethernet, UART, SPI, I²S, I²C), the R-Car E1 SoC can handle further external devices and can be linked into common automotive networks.
Refer to the separate sheet for the main specifications of the R-Car E1 SoC.
Pricing and Availability
Samples of Renesas' R-Car E1 SoC are available now, equipped in a 429-pin BGA (ball grid array) package, priced at US$30 per unit. Mass production is scheduled to begin in June 2012, and at a rate of 100,000 units per month in June 2013. (Pricing and availability are subject to change without notice.)
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks) ARM and Cortex are registered trademarks or trademarks of ARM Limited. PowerVR SGX is a registered trademark of Imagination Technologies in the EU and other countries. Other product and service names that appear in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.