Skip to main content

Renesas Electronics Expands Ground-Breaking IoT Platform with Renesas Synergy™ Software Package, S7G2 Microcontrollers and the First Verified Software Add-On for the Platform

January 13, 2016

TOKYO, Japan, January 13, 2016 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced new developments for the Renesas Synergy™ Platform, including the commercial release of the Renesas Synergy Software Package (SSP) version 1.0.0, mass production availability of the S7G2 Renesas Synergy Microcontrollers (MCUs), and availability of the first Verified Software Add-on (VSA) software from VSA Program partners.

The Renesas Synergy Platform, winner of the 2015 Elektra Internet of Things Product Innovation Award (Note 1), is a complete and qualified platform for the development of embedded and IoT applications. It was designed to provide engineers with a platform that already has basic system elements implemented, configured and tested, so engineers can eliminate the time normally needed to implement and integrate base-line functionality and move almost immediately to product design, potentially reducing time to market by months. This allows system manufacturers to truly differentiate and increase the value of the end product they create.

The SSP, the core of the Renesas Synergy Platform, integrates a real-time operating system with a rich set of utilities, drivers, libraries, software stacks, and application framework — all optimized specifically for the Renesas Synergy MCU architecture and fully supported by Renesas. The 1.0.0 version is the first version of the SSP fully qualified and usable in products in mass production.

The first devices in the Renesas Synergy Family of MCUs to go into mass production, the S7G2 Group of MCUs provides a high-performance CPU core and a large flash memory size for high-performance human machine interface (HMI) applications.

Cypherbridge Systems, Icon Labs, and Skkynet, all members of the VSA Program, are the first program members to offer production-ready software for the platform via the Renesas Synergy Gallery, the comprehensive online source for the Renesas Synergy Software.

For more information about the Renesas Synergy Platform and VSAs, please visit http://www.renesassynergy.com.

(Note 1) About the 2015 Elektra Internet of Things Product Innovation Award, please visit http://www.elektraawards.co.uk/elektraawards2015/2015-winners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

Renesas Synergy is a trademark of Renesas Electronics Corporation. All other registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on