New RS-485/422 Differential Transceivers Deliver ±5000V EFT Immunity and up to ±16,000V ESD Immunity for Industrial and Automation Applications

October 14, 2021

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced the RAA78815x Family of 5V differential RS-485/422 transceivers with industry-leading electrical fast transient (EFT) immunity ±5000V and ESD protection up to ±16,000V, making these products the ideal solution for noise-sensitive industrial communication networks. The six new full and half duplex ruggedized devices meet both the RS-485 and RS-422 communication standards and are ideally suited for a variety of industrial network, process control network, building automation, long-haul network, and security camera network applications.

The new devices build on Renesas’ current ISL315x 5V RS-485 transceiver family with additional immunity for EFT. In addition to the industry’s highest EFT immunity, the RAA78815x family delivers exceptional differential output voltages, featuring 3.1V into the RS-485-required 54Ω load. The new high-speed transceivers also feature bus leakage currents of maximum 125 μA, representing a true 1/8 unit load to the RS-485 bus. Developers can connect up to 512 transceivers on the same bus without using repeaters and without compromising the RS-485 network standard’s 32-unit load maximum. As a result of these changes, the RAA78815x family can lower implementation and downtime costs, since a single network can support more nodes with lower likelihood of communications issues due to ESD and EFT overvoltage transients.

“EFT immunity is mission critical for devices operating in harsh industrial and automation environments, such as HVAC, factory, and smart grid equipment, where devices are frequently turned on and off or added and disconnected from the system” said Bobby Matinpour, Vice President of the Standard Products Business Division at Renesas. “Featuring superior EFT immunity, output drive, and supply current levels, the RAA78815x family builds on 50 years’ experience in RS-485/422 transceiver design to deliver robust solutions for industrial and factory automation.”

Key Features of the RAA78815x Family

  • ±5000V EFT immunity
  • ±16,000V ESD immunity
  • 3.1V (typ) into Rd = 54Ω
  • Low 125 μA bus current, 550 μA supply current, and 70nA shutdown current
  • Ultra-small 3x5 mm MSOP and 6 x 8.6 mm SOIC package
  • Support for multiple data rates and both full (RAA788150, RAA788153, and RAA788156) and half (RAA788152, RAA788155, and RAA788158) duplex modes

The new RAA78815x transceivers are optimal solutions for high-reliability systems. Renesas has designed multiple system architectures using complementary power, analog, and microcontroller offerings to create comprehensive solutions for a variety of applications, including the 48V Position Control Solution and AC Servo Motor Control with Industrial Network Connections, among many others. Renesas’ Winning Combinations are vetted solutions engineered to help customers accelerate designs and get to market faster. Renesas offers more than 250 Winning Combinations that work together seamlessly for a wide range of applications and end products. They can be found at renesas.com/win.  

Availability

The RAA78815x transceivers are available now in MSOP and SOIC packages with pin counts ranging from 8 to 14. An evaluation board for the new transceiver family is also available. For more information, please visit https://www.renesas.com/eftprotection.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube and Instagram.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on