TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced a new industry-leading Bluetooth chip that combines a radio transceiver, an Arm® M0+ microcontroller, memory, peripherals and security features in a compact SoC design. The DA14533, the first automotive-qualified device in the company’s Bluetooth® Low Energy system-on-chip (SoC) family, includes advanced power management features to simplify system integration and reduce power consumption. With its software stack qualified against Bluetooth Core 5.3 and support for extended temperatures, developers can jump-start projects in applications from tire pressure monitoring and keyless entry to wireless sensors and battery management systems.
Optimized Design to Deliver Unparalleled Power Efficiency
Building on Renesas’ leadership in Bluetooth LE SoCs (SmartBond Tiny Family) with industry-leading low power consumption, the new DA14533 includes some of the most advanced power management features in the industry. The device includes an integrated DC-DC buck converter, which accurately adjusts the output voltage according to system requirements. Active system power consumption is lower than comparable devices in the market, requiring only 3.1mA during transmission and 2.5mA during reception. In hibernation mode, the current drops to 500nA. These power management and power-saving features help extend the operational life of small-capacity battery-powered systems and meet the stringent power requirements of tire pressure monitoring systems’ mission profile.
Auto-Grade AEC-Q100 Qualified and Up-to-Date Security Features
The DA14533 is an AEC-Q100 Grade 2 qualified device, which means the device has passed strict testing to sustain quality and reliability in harsh automotive environments. Moreover, the device’s extended temperature range (-40 to +105°C) ensures reliable performance in demanding conditions, making it ideal for automotive and industrial systems where stability and durability are essential. Qualified against Bluetooth Core 5.3 specifications, the device contains the latest security features to safeguard connected devices from various threats.
“Our SmartBond Tiny SoC family has seen remarkable success in the industrial market, with over 100 million units shipped to date,” said Chandana Pairla, VP of Connectivity Solutions Division at Renesas. “This new automotive-grade device will enable a new class of Bluetooth LE applications that demand high power efficiency, a small footprint and broader temperature tolerance for next-generation battery-powered automotive and industrial systems.”
Lower Bill-of-Materials Reduces Costs and Simplifies Development
Similar to other Bluetooth LE SoC devices in the SmartBond Tiny family, the DA14533 only requires 6 external components, offering a best-in-class engineering bill of materials (eBOM).
A single external crystal oscillator (XTAL) is used for both active and sleep modes, eliminating the need for a separate oscillator for sleep mode. Its ultra-compact design – available in a WFFCQFN 22-pin 3.5 x 3.5 mm package – makes the device the smallest automotive Bluetooth LE SoC on the market. With its compact design and low eBOM, the device integrates seamlessly into space-constrained systems, reducing overall system costs and accelerating time-to-market for customers.
Key Features of the DA14533
- Arm® Cortex®-M0+ microcontroller – Standalone application processor or data pump in hosted systems
- 64KB RAM and 12KB One-Time Programmable (OTP) memory
- 2.4 GHz radio transceiver
- Integrated low IQ buck DC-DC converter
- External SPI flash
- Single XTAL operation (single crystal oscillator)
- Software stack qualified against Bluetooth Core 5.3
- AEC-Q100 Grade 2-qualified with wide operating temperature range support (-40 to +105°C)
- WFFCQFN 22-pin 3.5 x 3.5 mm package
Winning Combinations
Renesas has combined the new Bluetooth LE SoC with the R-Car H3/M3/E3 SoCs, PMICs, and timing devices to offer a wide array of Winning Combinations including “Tire Pressure Monitoring System.” Winning Combinations are technically vetted system architectures from mutually compatible devices that work together seamlessly to bring an optimized, low-risk design for faster time to market. Renesas offers more than 400 Winning Combinations with a wide range of products from the Renesas portfolio to enable customers to speed up the design process and bring their products to market more quickly. They can be found at renesas.com/win.
Availability
The DA14533 is available today, along with the Bluetooth Low Energy SoC Development Kit Pro. The kit includes a motherboard, daughterboard, and cables to facilitate application software development. The daughterboard is also available by itself to simplify development. A blog about the new device is available. More information about Renesas Bluetooth Low Energy solutions is available at: renesas.com/products/wireless-connectivity/bluetooth-low-energy
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, X, YouTube, and Instagram.
(Remarks) Bluetooth is a registered trademark of Bluetooth SIG, Inc. of the United States. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.