New Environment Allows Customers to Bring Leading-Edge Software to Market Quickly
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the launch of a virtual development environment that enables advance development and operational evaluation of automotive application software to support the latest requirements of electrical/electronic architecture (E/E architecture). The environment includes a Virtual Turnkey Platform, which allows engineers to develop application software before devices or evaluation boards are available. Additionally, the new environment offers a Multicore Debug and Trace Tool, which enables users to analyze and evaluate the operation of their software as if it were running on an actual chip. These tools will allow customers to kick-start development and get to market faster with leading-edge software.
“With the evolution of E/E architecture, there is an increasing demand for software design that can maximize performance at a system level. At the same time, the increasing time and cost associated with software development have become a big challenge,” said Hiroshi Kawaguchi, Vice President, Automotive Software Development Division at Renesas. “Our integrated software development environment that can be used across gateway systems, ADAS, and xEV development, enables customers to benefit from the scalability of Renesas products such as R-Car and the RH850 family for both software and hardware development.”
As software becomes a critical part of automobiles, customers’ application software becomes larger and more complex. In order to increase the value of their software, customers are looking for new development methods and environments to develop highly reliable software more quickly.
“Virtual Turnkey Platform” Application Software Development Environment
This platform consists of the R-Car Virtual Platform (R-Car VPF) development environment and a software development kit (R-Car SDK) that includes pre-tested software libraries and sample code. R-Car VPF is based on Virtualizer Development Kits (VDKs) from Synopsys, and integrates virtual models of intellectual property (IP) specific to R-Car to customize for R-Car devices. By overlaying the R-Car SDK on this platform, it enables engineers to immediately start development of application software virtually. The platform accurately recreates the behavior of the actual chip and thus eliminates the need to build up a development environment with a physical evaluation board. Multiple users can also develop software simultaneously on separate PCs or servers.
“Multicore Debug and Trace Tool” for Analyzing and Evaluating Software Operation
Once engineers complete the development of multiple software components side by side on the Virtual Turnkey Platform, the next step is to integrate the software and verify that it runs on a single chip. Software components share resources such as the multiple CPUs and IPs on R-Car SoCs. If operational problems are detected after the software components are integrated, it requires a tremendous amount of work to analyze and solve these issues. With this in mind, Renesas created the Multicore Debug and Trace Tool, which simplifies the process of analyzing and identifying the causes of errors occurring from the interaction of the multiple hardware resources in R-Car SoCs. This enables synchronous and simultaneous debugging of the entire heterogeneous architecture of R-Car without using the actual device. This helps identify potential problems and thus accelerates the development process.
Availability
The development environment is available for the R-Car S4 SoC for automotive gateways. Renesas has plans to support the R-Car V4H as well as future versions of R-Car products and RH850 automotive MCUs.
For more information on the Virtual Turnkey Platform, please visit:
https://www.renesas.com/products/automotive-products/automotive-system-chips-socs/virtual-turnkey-platform.
For more information on the Multicore Debug and Trace Tool, please visit:
https://www.renesas.com/software-tool/multi-core-debug-and-trace-tool.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) empowers a safer, smarter and more sustainable future where technology helps make our lives easier. A leading global provider of microcontrollers, Renesas combines our expertise in embedded processing, analog, power and connectivity to deliver complete semiconductor solutions. These Winning Combinations accelerate time to market for automotive, industrial, infrastructure and IoT applications, enabling billions of connected, intelligent devices that enhance the way people work and live. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, YouTube, and Instagram.
(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.