Transphorm Inc.—the leader in the design and manufacturing of the highest reliability and only qualified high-voltage (HV) Gallium Nitride (GaN) semiconductors—today confirmed that leading power supply manufacturer TDK-Lambda, a group company of TDK, has released its first GaN-based AC-DC power supply. The full function 504 W rated PFH500F-28 is the company's latest generation AC-DC baseplate cooled power supply module. Further, the power module is the latest Transphorm customer product to demonstrate the HV GaN advantages, increasing efficiency by 5 percent in a 28 percent smaller package over the previous PFE500F series.
Broad Industrial Applications Get a Boost
The PFH500F-28 is a low-profile power module with 28 volts of output power designed for various harsh environment applications, commercial off-the-shelf (COTS) power supplies, custom fanless power supplies, traffic signaling, and more. TDK-Lambda's redesigned standard power module uses a bridgeless totem-pole power factor correction topology to optimize Transphorm's TPH3206LDG FET in the popular 8x8 PQFN package.
The development project was led by the TDK-Lambda Americas Dallas, TX team and leveraged Transphorm's application support team throughout various phases of the three-year initiative.
"We are excited to introduce the new standard PFH series," explained Jin He, Vice President of Engineering at TDK-Lambda. "Our engineers diligently review new technologies that will benefit our end customers to ensure any new product we release is reliable and a notable advancement over prior models. Our decision to work with Transphorm on our first GaN AC-DC product was based largely on the power semiconductors' proven quality and reliability as well as the team's reputation for successful collaboration. Our experience was such that we've released the PFH500F-28 with our three year warranty and are in discussions with Transphorm regarding future projects."
Transphorm's GaN to date has enabled customers to produce computing power supplies, servo motors, and telecom power supplies that show marked advantages in power density, size, and system cost. TDK-Lambda's power module joins them as the PFH500F-28 delivers the following advantages when compared to its Silicon-based predecessor:
- Power efficiency: up to 92 percent, a 5 percent increase over the PFE500F
- Power density: 100W/cubic inch, a 30 percent increase over the PFE500F
- PMBus™ monitoring and programming (read/write)
- Size reduction: From 122 x 70 x 12.7 to 101.6 x 61 x 13.5mm, a 28 percent reduction
- Reduced size of external capacitive components
- Thermal impact: 38 percent reduction in waste heat, requiring less heatsink/cooling than the PFE500F
About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, and magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, Micronas, Tronics and TDK-Lambda. TDK's further main product groups include magnetic application products, energy devices, and flash memory application devices. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2018, TDK posted total sales of USD 12 billion and employed about 103,000 people worldwide.
About TDK-Lambda Corporation
TDK-Lambda Corporation, a group company of TDK Corporation, is a leading global power supply company providing highly reliable power supplies for industrial equipment worldwide. TDK-Lambda Corporation meets the various needs of customers with our entire range of activities, from research and development through to manufacturing, sales, and service with bases in five key areas, covering Japan, Europe, America, China, and Asia. For more details, please visit https://www.tdk-lambda.com/en/.
Welcome to the GaN Revolution!
Transphorm designs and manufactures the highest performance, highest reliability GaN semiconductors for high-voltage power conversion applications. Holding one of the largest IP portfolios (600+ patents), Transphorm produces the industry's only JEDEC and AEC-Q101 qualified GaN FETs. This is due to a vertically-integrated business approach, which allows for innovation at every development stage: design, fabrication, device, and application support. Transphorm: moving power electronics beyond Silicon limits. Website: transphormusa.com Twitter: @transphormusa
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.