Skip to main content

[UPDATE 3] Renesas Electronics Announces Resumption of Wafer Lines Production at Naka Factory, Moves Up the Schedule for Shipment of Products from October to September

June 10, 2011

TOKYO, Japan, June 10, 2011 — Following the announcement made on May 11, 2011, Renesas Electronics Corporation (TSE: 6723) today released an updated production schedule for its Naka wafer fabrication factory in Hitachinaka, Ibaraki. Having resumed mass production at both the 200- and 300-mm wafer fabrication lines, the key highlight of the new schedule is that Renesas expects it will be capable of significantly moving up the schedule by one month from the end of October to the end of September for when the supply (shipment) capacity will return to pre-earthquake levels.

The second preliminary schedule includes two updates as follows:

(1) Schedule for mass production at both the 200- and 300-mm wafer fabrication lines

Renesas began test production on the 200-mm (8-inch) and 300-mm (12-inch) wafer fabrication lines on April 23 and April 25, respectively, and has achieved the same results as pre-earthquake levels in quality and reliability testing, etc. Subsequently, Renesas succeeded in resuming mass production of both the 200-mm (8-inch) and 300-mm wafer fabrication lines from June 1 and June 6, respectively, as scheduled.

(2) Expected timing on when the shipment capacity will return to that of pre-earthquake levels with additional supply from Renesas Group's other factories and outside foundries

Having further accelerated the restoration steps for part of the manufacturing equipment at the Naka factory, Renesas now expects it will be capable of significantly moving up the schedule of when the shipment capacity will return to that of pre-earthquake levels with additional supply from other factories and outside foundries, from the end of October to the end of September.

Renesas Electronics will continue to focus all possible effort on the recovery work at the Naka factory. The company expresses gratitude for all the support it received from companies outside the Renesas Group, which helped to speed up the resumption of operation and move up the production schedule.

(Note) While it is the company's intent to follow the above schedule to the best of its ability, the published dates may change. The schedule assumes a stable source of electrical power and no further damage from subsequent aftershocks.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on