Skip to main content

MoSys and IDT Collaborate to Deliver 100 Gbps Base Station, Data Center and Mobile Edge Computing Solutions Leveraging RapidIO Technology

LineSpeed Flex 28G MUX Doubles IDT RapidIO Switch Port Density for Backplane or 100G QSFP Applications

November 9, 2016

SANTA CLARA and SAN JOSE, Calif., Nov. 9, 2016 – MoSys (NASDAQ: MOSY), a leader in semiconductor solutions that enable fast, intelligent data access for Cloud, network, and communications systems, and Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), today announced interoperability between MoSys’ new LineSpeed™ Flex 28G 2:1 MUX IC (MSH420) and IDT’s 24-Port, 48-Lane, 600 Gbps, 10xN RapidIO® Switch (RXS2448). The IDT® Switch delivers ultra-low latency and high-bandwidth in both wireless and wireline 100G, 400G, and terabit network infrastructure applications, such as mobile edge computing, high-performance computing, and data analytics. The MoSys® LineSpeed Flex 28G MUX and retimer protocol independent devices are compatible with the 10G or 12.5G RapidIO interfaces and enable a reduction in backplane traces or QSFP cable counts for high density RapidIO systems.

Combining the MSH420 bit interleaved MUX and the RXS2448 RapidIO switch, users can build high-speed, low-latency RapidIO networks with half the number of backplane or QSFP interconnects.   The combination of rates allows customers to leverage the expanding 100G QSFP interconnect ecosystem.

The solution:

  • Builds on IDT 50 Gbps per port silicon
  • Muxes multiple 12.5 Gbps lanes into single 25 Gbps lane to deliver up to 100 Gbps per port over cable or backplane
  • Provides system-level savings in cost and cables
  • Leverages tight interoperability between IDT Switching silicon and MoSys MUX PHY IC

The MoSys MSH420 MUX PHY IC is a flexible SerDes device designed to MUX high-speed protocols into a higher rate output in one direction and DeMUX in the other direction. The device bit interleaves protocol independent rates ranging from 10-14G into a single stream at 2 times the rate.  In a typical application, the device will MUX and DeMUX 8 lower speed lanes to 4 at double the data rate. Using a unique training capability, the device can maintain lane ID from point to point. For RapidIO, each pair of 10G or 12.5G data streams is combined into 20G or 25G, making the device ideal for a broad range of bandwidth consolidation applications, such as increasing backplane density or consolidating 8 12.5G links into 4 25G links to leverage the QSFP28 ecosystem.

IDT’s 10xN RXS2448 RapidIO switch offers ultra-low port-to-port latency approaching 100ns and a flexible, non-blocking fabric with switching performance of up to 600 Gbps to deliver an optimized high-speed switching solution. The new switches are backward-compatible with existing RapidIO ecosystems, protecting previous hardware and software investments while accelerating time to market.

“Mobile edge and data analytics applications require extremely high-speed, low latency movement of data in order to meet the performance requirements of the complex electronic systems within the mobile network infrastructure,” stated Sean Fan, vice president and general manager, Computing and Communications Division at IDT. “IDT’s latest RXS2448 RapidIO switch and the MoSys’ LineSpeed Flex MUX technology deliver these capabilities with higher density, lower power and a reduced number of cables. “

“IDT’s RapidIO switching solutions have a proven track record as a low-latency interconnect in the mobile edge and other expanding applications,” stated John Monson, VP of marketing and sales for MoSys. “The MoSys 28G protocol-agnostic 2:1 MUX allows customers to scale in performance and density at low cost and to risk leverage a proven and expanding 25G and 100G ecosystem for backplane and module interconnect.”

About MoSys, Inc.

MoSys, Inc. (NASDAQ: MOSY) is a fabless semiconductor company enabling leading equipment manufacturers of Cloud, networking, communications, and data center systems to address the continual increase in Internet users, data and services. The company's solutions deliver data path connectivity, speed and intelligence while eliminating data access bottlenecks on line cards and systems scaling from 100G to multi-terabits per second. Engineered and built for high-reliability carrier and enterprise applications, MoSys' Bandwidth Engine®, Programmable Search Engine, and LineSpeed™ IC product families are based on the company's patented high-performance, high-density intelligent access and high-speed serial interface technology, and utilize the company's highly efficient GigaChip® Interface. MoSys is headquartered in Santa Clara, California. More information is available at www.mosys.com.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, timing, wireless power transfer, serial switching, interfaces, automotive ASICs, battery management ICs, sensor signal conditioner ICs and environmental sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT can be found at www.IDT.com. Follow IDT on FacebookLinkedInTwitterYouTube and Google+.

Bandwidth Engine, GigaChip, and MoSys are registered trademarks of MoSys, Inc. in the US and/or other countries. IC Spotlight, LineSpeed and the MoSys logo are trademarks of MoSys, Inc. All other marks mentioned herein are the property of their respective owners.

© 2016, IDT. IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on