Skip to main content

Renesas Electronics' ADAS Surround View Kit Accelerates Development of Surround View Applications

October 8, 2015

TOKYO, Japan, October 8, 2015 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the ADAS Surround View Kit. Given the increasing complexity of ADAS (Advanced Driver Assistance System) systems, Renesas is committed to providing easy-to-use solutions that enable quick time to market for automotive system manufacturers. On July 16, Renesas introduced its ADAS Starter Kit, designed to be used in a wide spectrum of applications. The new ADAS Surround View Kit, an extension of the ADAS Starter kit, simplifies and accelerates the development of surround view applications when combined with the ADAS Starter Kit in particular. Surround view applications are expected to play a major role in future cars, providing additional comfort and new safety features.

The ADAS Surround View Kit combines automotive cameras from Integrated Micro-electronics Inc. and multiple high-speed gigabit multimedia serial links (GMSL) from Maxim Integrated Products, Inc. on a miniature automotive chassis. This eliminates the need for system manufacturers to source and set up all these specific automotive components themselves for their surround view development.

The kit also provides a 2-channel CAN interface and a gigabit Ethernet connector interface for in-car applications, where the model chassis is not used.

Once connected via an on-board extension connector to the already available ADAS Starter Kit, the ADAS Surround View Kit provides outstanding processing performance to system manufacturers. It is based on the cutting-edge performance of Renesas' R-Car H2 SoC (System-on-Chip), which is capable of delivering more than 25,000 DMIPS and providing state-of-the-art 3D graphics capabilities and powerful vision processing cores. The R-Car H2 SoC supports up to four independent input HD camera channels, allowing easy implementation of 360° camera views and object recognition.

The new kit is supported by the Yocto distribution that is also used for other R-Car evaluation boards. In addition, Renesas will provide sample applications that will help system manufacturers to use the ADAS Surround View Kit quickly and easily, and accelerate the development of dedicated hardware and software solutions for future ADAS applications.

Availability

The ADAS Surround View Kit is available now, with shipping scheduled to begin in December 2015. The Yocto distribution and initial support is available now on the Embedded Linux Wiki website: http://elinux.org/ and on the Renesas Engineering Community. (Availability is subject to change without notice.)

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

All registered trademarks or trademarks are the property of their respective owners


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on