TOKYO, Japan, March 13, 2013 — Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, has developed a new split gate (SG) flash memory circuit technology for on-chip flash memory microcontrollers (MCUs) that adopts the industry's leading-edge 40 nanometer (nm) process technology achieve high reliability, low power consumption and the industry's fastest random access operation speeds.
In addition to higher level control, equipment that requires high reliability, e.g., automotive, is also now requiring even higher functionality and diversity of functions, such as support for functional safety, security, and networking. Along with such market demands, since even larger capacities are required in the flash memory that stores the MCU's software and data, it is seen as desirable to increase the integration density of both the flash memory and peripheral functions included on a single chip by the use of even finer features in the fabrication process.
To support these needs, Renesas continues to develop leading-edge solutions based on advanced process technologies, and starts sample shipments from 2Q CY2013 of automotive flash MCUs that adopt both the industry's leading-edge 40nm process for flash MCUs and the SG-MONOS structure [Note *] flash memory, which has a proven track record in terms of high reliability, high speed, and low power consumption.
Key Features of the Newly-Developed SG-MONOS Flash Memory Technology:
(1) Circuit technologies achieve even faster readout
If the offset voltage of the sense amplifier that amplifies the read data is large, the time for reading data from the cell will be correspondingly long. Renesas has developed a sense amplifier that can largely cancel the offset voltage using a correction current, thus increasing the random access speed.
(2) Circuit technologies achieve high rewrite durability
Renesas has developed a variable control method that, during write operations, adapts the current applied to the cell according to the progress of the write operation. Renesas also developed a technology for use during erase operations, dynamically controlling the pulse application time to be optimal by monitoring the voltage level applied to the cell. These two developments enable faster rewrite operations and reduce the voltage stress applied to the cell during rewrite, thus allowing the number of rewrite cycles to be increased.
Using these new technologies, Renesas has prototyped both 4 MB program storage flash memory and a 64 KB data storage flash memory fabricated in a 40nm generation process, and has achieved operation at over 160 MHz and high readout speed of 5.1 GB per second—the industry's highest speed for program storage flash memory. Previously, Renesas verified operation at up to 120 MHz in its 40nm generation process products. Leveraging these new technologies, Renesas has now verified a 33% characteristics improvement. Also, in data storage flash memory, this technology achieved 10 million rewrite cycles, a critical issue in automotive MCUs, even under the high-temperature conditions of Tj = 170℃. This indicates that Renesas 40nm automotive flash memory has great potential in terms of rewrite cycle counts.
Renesas is hopeful that using this flash memory circuit technology can contribute significantly to creating automotive flash memory that provides even higher performance and reliability.
Renesas presented these results on February 19 during a session at ISSCC 2013 (International Solid-State Circuits Conference 2013), which took place in San Francisco, February 17-21, 2013.
[Note *]: MONOS (metal oxide nitride oxide silicon): A memory transistor (memory cell) structure in which there is a three-layer oxide/nitride/oxide structure formed on a silicon substrate and the control gates (metal) are formed on top of that. Over 20 years ago, Renesas included MONOS technology in IC card memory products. Based on this proven track record, Renesas developed SG-MONOS, which is a MONOS technology in which the gate electrode is split into two to form a split gate (SG), and is now incorporating this technology in MCUs as an SG-MONOS type flash memory, which achieves high reliability, high-speed operation and low power consumption.
(Remarks)
All product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.