Enables Up to 100W Power Supply over a USB Interface for Industrial, Home Appliance, and OA/ICT Applications

June 2, 2014

TOKYO, Japan, June 2, 2014 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced its new Universal Serial Bus (USB) Power Delivery (PD) controller (part number μPD720250) that is based on the USB PD Specification to deliver up to 100W (5 A at 20 V) power over a USB PD cable. Renesas will exhibit its new USB PD controller at Computex Taipei from June 3 to June 7, 2014 at booth # N0608, 4th floor of the Nangang exhibition hall in Taipei.

By combining the new USB PD controller with an optimal power supply circuit, designers will be able to rapidly implement USB-based solutions that provide higher power to notebook PCs and also can reduce the battery charging time for smartphones and tablets. Furthermore, by standardizing the AC adapters provided with notebook PCs and other equipment, both development costs and design challenges can be reduced.

Smartphones and tablet PCs are demanding increasingly larger power supplies. To address this market need, the USB PD Specification was developed by the USB 3.0 Promoter Group in 2012 to allow equipment with large power requirements, such as notebook PCs, to be powered over a USB connection. In the USB PD Specification, the connected equipment can mutually negotiate power supply capacities and requirements and then, after safety has been verified, the USB circuits can control the power supply up to 100 W; up from the previous 7.5 W level. The newer 100W power supply adequately supports high-power consumption equipment and significantly reduces battery charging times.

Furthermore, the earlier USB power supply was limited to unidirectional supply from host/hub equipment to peripheral equipment; in the USB PD Specification, the power supply is bidirectional and power can be sent in either direction. This is expected to allow the creation of new applications. For example, at the same time as video is being output on a large-size monitor over a USB connection from a notebook PC, the USB PD Specification will allow the large-size monitor, which is powered from the AC power mains, to supply power to the notebook PC, which is being operated on battery power.

Key features of the new USB PD controller:

(1) Based on the USB PD Specification

The μPD720250 USB PD controller is based on the USB PD Specification and in addition to supporting both the power supply and the power receiving sides of a USB connection, can flexibly support either role depending on the actual conditions of operation.

(2) Provision of optimal solutions for all types of system

The µPD720250 device is capable of control over an SMBus (Note 1) and can be easily incorporated into tablets and notebook PCs. It also provides flexible support for external ROM firmware and can thus implement optimal systems for both the power supply and power receiving sides. Furthermore, Renesas plans to provide powerful support for system development by offering solution kits that include both boards and software for all types of system.

(3) Low-power consumption to support Energy Star (Note 2) and the EuP Directive (Note 3)

The μPD720250 device takes advantage of Renesas' low-power technologies for reductions of both standby and operating power consumption and is appropriate for the Energy Star and the EuP Directive.

(4) Built-in regulator and compact package

The μPD720250 device includes an integrated 1.0 V regulator and can operate from a single 3.3 V power supply. It is provided in a compact package and enables lower costs and miniaturization in system construction.

Refer to the separate sheet

for the specifications for the new µPD720250 PD controller.

(Note 1) SMBus:
A serial interface specification for connecting the various components within a personal computer and transmitting the information necessary for power supply management.

(Note 2) Energy Star:
An environmental labeling system for energy-saving electrical equipment products promoted by the United States and operated in Japan, Australia, Canada, the EU, and other countries and areas.

(Note 3) EuP Directive:
A European Union environment system that aims at evaluating the environmental burden over the whole product life cycle and reducing that burden.

Leadership in USB

As a member of the USB Implementers Forum (USB-IF) since 1996, Renesas (formerly NEC Electronics) has played a leading role both in defining USB standards and developing USB technology. In April 2000, the company (then NEC Electronics) launched the world's first USB 2.0-compliant host controller chip (uPD720100), the world's first USB 2.0-compliant hub controller chip (uPD720110) and an extensive lineup of other USB devices. Renesas has earned a reputation for delivering dedicated customer service and high quality. In May 2009, Renesas (then NEC Electronics) introduced the industry's first USB 3.0 xHCI host controller (uPD720200) and earned the first “Certified SuperSpeed USB (USB 3.0)” certification from the USB-IF. With the robust and compliant design of uPD720200, Renesas contributed to the USB-IF certification tests, providing the organization with a host controller product as the platform for other USB 3.0 peripheral devices to perform interoperability testing.

Availability

Samples of Renesas Electronics' μPD720250 will be available in July 2014. (Availability is subject to change without notice.)

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks)
All other registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on