Skip to main content

Renesas Electronics Completes the Initial Span of Microcontrollers in its Industry-First Renesas Synergy™ Platform by Adding Three New MCU Groups

S128, S3A3, and S3A6 Groups Achieve Full Portfolio Coverage of Scalable and Compatible Synergy MCUs within the Synergy Platform

November 4, 2020

Tokyo, Japan, March 29, 2017 – Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced that it is extending its microcontroller (MCU) portfolio within the Renesas Synergy™ Platform to cover an even wider range of capabilities, CPU performance, and memory sizes, so system developers can get exactly what they need to create innovative solutions that drive their businesses. This expanded spectrum of scalable and compatible MCUs provides developers with several options to develop end-use products with a high degree of re-use of engineering resources in both hardware and software.

With the addition of the new S128, S3A3, and S3A6 Groups of Synergy MCUs, there are now a total of seven MCU Groups with 57 devices based on ARM® Cortex®-M CPU cores covering operating frequencies ranging from 32MHz up to 240MHz, and on-chip flash memory sizes of 64KB, 128KB, 256KB, 512KB, 1MB, 2MB, and 4MB. Renesas will continue to add new Synergy MCU Groups in the future, building on this foundation to increase the depth of solutions for specific applications.

The 20 new Synergy MCU devices in the S128, S3A6, and S3A3 Groups are sampling now to select customers and will be available to the general market in June 2017. For an early access to these MCUs’ information, join the Renesas DevCon Japan 2017 in Tokyo, on April 11.

Since its introduction to the market in October 2015, Synergy Platform capabilities have grown in software with the expansion of the Synergy Software Package (SSP) and its unprecedented levels of software quality assurance through:

  • Partner solutions with more Verified Software Add-Ons (VSAs)
  • Software development tools with the inclusion of the IAR Embedded Workbench® for Renesas Synergy™
  • Hardware with new Synergy Kits
  • More MCU devices that are fully accessible through the Application Programming Interface (API) of the SSP

The continual growth of the Synergy Platform inspires system developers to innovate more embedded control and Internet of Things (IoT) applications by reducing the obstacles that might prevent them from starting new designs. Because of this platform approach to development, companies enjoy a significant reduction in time to market and a lower total cost of ownership over the life of their products.

“Over the last eighteen months, the Synergy Platform has grown, as a comprehensive platform, to help realize our goal of adding real value for our customers in every step of their journeys,” said Peter Carbone, Vice President of Synergy IoT Platform Business Division, Renesas Electronics Corporation. “With the addition of these latest three MCU Groups, the MCU portfolio of the Synergy Platform now covers the entire selection range of memory and package sizes our customers request, and we provide the ability to easily scale up and down between them, which includes software and tools to reduce re-design efforts. These are core principles of the Synergy Platform that support reducing time-to-market and lowering the total cost-of-ownership for our customers”.

S128, S3A3, and S3A6 Group MCU devices

System developers with leaner requirements can select devices from the S3A3 and S3A6 Groups having 512 KB and 256 KB flash memory in a larger selection of the Synergy MCU Groups that provides more options to meet their end-use products’ requirements. The S128 Group also extends selections for ultra-low power applications that require larger memory up to 256 KB or require additional analog signal conditioning.

Renesas will showcase several demonstrations of the Synergy Platform’s recent innovations, including the latest Synergy Software Package (SSP) version 1.2.0, the Wi-Fi Framework, and its secure manufacturing reference solution with the recently introduced Synergy S5D9 Group of secure MCUs, at Renesas DevCon Japan 2017 in Tokyo on April 11. To learn more about the Renesas Synergy Platform, visit www.renesassynergy.com.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and/or elsewhere. IAR embedded Workbench is a registered trademark of IAR Systems. X-Ware is a trademark of Express Logic, Inc. Renesas Synergy is a trademark of Renesas Electronics Corporation. All other registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on