Skip to main content

Renesas Electronics Delivers 8.48 MP CMOS Image Sensor for 4K Network Security Cameras

Renesas Enters the Market for CMOS Image Sensors for High-End Network Security Cameras

November 4, 2020

TOKYO, Japan, August 30, 2017 - Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced a new high-sensitivity, high-resolution 8.48 megapixel (MP) CMOS image sensor (RAA462113FYL) that supports 4K video cameras. In conjunction with the existing Renesas 2.12 MP product that is already in mass production, Renesas will be providing full-scale sales support for its high-end CMOS image sensor for network security cameras.

To meet the increasing needs for network security cameras in financial institutions, transportation systems and commercial establishments, the new CMOS image sensor provides functions appropriate for imaging under the varied environmental conditions required by high-end devices and contributes to increased system performance.

Key features of the new CMOS image sensor

  • Achieves excellent low-light performance
    The new sensor achieves clear, high-visibility full-color imaging even in a moonlit environment
  • High resolution at high data rate
    The new sensor captures clear, high-visibility images even when digital zoom is used due to its capture of high-reliability 4K video at 60 fps.
  • High dynamic range
    The new sensor supports a line-by-line HDR (high dynamic range) mode in which long exposure data and short exposure data are output separately for each line. This allows video capture, even for high-contrast scenes.

Renesas also provides a reference board that was developed together with a camera module manufacturer to allow users to evaluate the performance of the Renesas CMOS image sensor. Renesas plans to work with camera module manufacturers to supply camera modules with a variety of features such as autofocus functions, HDR (high dynamic range) functions, wide-area monitoring functions, and vibration reduction (image stabilization) functions. This will allow system manufacturers to reduce the development period and development costs for new high-performance network security camera products.

Renesas will continue to expand its line of security camera solutions for network security cameras, by providing its CMOS image sensors in combination with microcontrollers (MCU).

Availability

Samples of the RAA462113FYL are now available and mass production is scheduled to begin in December 2017. (Availability is subject to change without notice.)

Refer to the separate sheet (PDF: 46 KB) for the main specifications of the RAA462113FYL.

For more information on the CMOS image sensor, please visit: https://www.renesas.com/en/products/analog/other-analog-ics/ics-for-camera.html

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on