New Technology Achieves Industry's Largest Capacity of Embedded Flash Memory – 24 MB – and Industry's Fastest Random Access Operation of 240 MHz

June 12, 2019

TOKYO, Japan ― Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the development of a new flash memory technology that achieves larger memory capacities, higher readout speeds, and over-the-air (OTA) support for automotive microcontrollers (MCUs) using the next-generation 28nm process. This new technology achieves the industry's largest capacity of embedded flash memory on an MCU – 24 MB – and reaches 240 MHz random access read speeds, the industry's fastest for embedded flash memory. The technology also achieves low noise write operations when performing OTA wireless software updates, and high-speed and robust operation for OTA software updates.

Renesas presented these results on June 12 at the 2019 Symposia on VLSI Technology and Circuits in Kyoto, Japan, June 9-14, 2019.

Recently in leading-edge technologies used in car systems, such as autonomous driving and electric drive, there have been increasing demands for larger embedded flash memory capacities in the MCUs due to the increasing scale of the control software. The introduction of OTA technology accelerates the demand for larger capacities to assure adequate storage area for updated programs. Since it is necessary to assure real-time performance given the addition of new functions such as functional safety, faster random access read times from the flash memory are also strongly desired. Furthermore, regarding OTA, three things are now strongly desired. First is low-noise design so that the updated software can be stored reliably even when the car is operating. Second is reduced down time during the software switching. Third is robustness to avoid incorrect operations even if unintentional interruptions occur when updating or switching software.

The newly developed flash memory technology addresses these demands with:

24 MB on-chip flash memory – the industry's largest in an MCU

Renesas continues to adopt the high-speed, high-reliability SG-MONOS (note 1) technology for the embedded flash memory used in its MCUs. The memory cell size of the 28nm generation developed here is reduced by more than 15 percent, from the earlier 0.053 µm² to smaller than 0.045 µm². While suppressing increases in the chip size, this new technology allows the inclusion of 24 MB of code storage flash memory, the industry's largest capacity for embedded flash memory. Renesas has also included 1 MB of data storage flash memory in the test chip for parameters and other data.

240 MHz random access read speed – the industry's highest speeds for MCUs with embedded flash memory

Word line division is an effective method for increasing the speed of random access reads in embedded flash memory. However, this division increases the number of word line drivers and causes reliability degradation due to time-dependent dielectric breakdown (TDDB) of the transistors included in those drivers and word line supply voltage drops due to increased leakage current. Renesas resolved these issues using word line driver stress mitigation and distributed word line supply voltage drivers and has verified 240 MHz high speed random access, the industry's highest in a test chip, over a wide temperature range (junction temperatures from -40°C to 170°C).

Development of noise-reducing technology

By changing the write current applied to each memory cell between initial operation and later operation when programming the flash memory, Renesas has reduced the peak current consumption from the external power supply (Vcc) by 55 percent without reducing the throughput compared to earlier Renesas devices. This suppresses the adverse influence of supply voltage noise on the MCU itself during OTA operations when the car is running. Renesas has also applied the idea of varying the write current to high-speed write mode, in which the number of simultaneously programmed cells is increased. As a result, the new device achieves high-speed programming at 6.5 MB/s in this mode. This makes it possible to suppress the increased test times associated with the large memory capacity.

OTA capable of control software switching that is both robust and high speed

In this test chip, the code storage flash memory is divided into a storage area for software in use and a storage area for updated software. This makes it possible to switch the software in less than 1 ms (1/1000 of a second) at ignition off. Furthermore, the software switching settings are duplicated and new state flags were added to prevent incorrect operation in the event that the software updates or switching is unintentionally interrupted. This achieves, at the same time, the robust operation that allows executable control software to be selected reliably and a reduction of down time during which the car cannot be used.

The above technologies make it possible to support the increasing scales of automotive control software, high-speed real-time control, and advanced OTA. Moving forward, Renesas is committed to continued development of embedded flash memory and striving to achieve the higher capacities, higher speeds, and lower power consumption that will be required to support new applications.

(Note 1) MONOS: Metal oxide nitride oxide silicon. A technology that Renesas has achieved a substantial track record of over 20 years in EEPROM, secure MCU, and other products. The MONOS technology is used in the embedded flash memory used in Renesas MCUs.

(Note 2) A Renesas flash memory technology announced at the 2015 International Solid-State Circuits Conference (ISSCC 2015).

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on