Skip to main content

Renesas Electronics Introduces Low-Cost Target Boards to Support Growing RX 32-bit MCU Family

Target Boards Jump Start Embedded Designs Using RX65N, RX130 and RX231 MCUs for Touch-Based Home Appliances, and Building and Industrial Automation Applications

November 4, 2020

TOKYO, Japan, February 19, 2018 – Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced three new Target Boards for the RX65N, RX130 and RX231 Microcontroller (MCU) Groups, each designed to help engineers jump start their home appliance, building and industrial automation designs. Priced below $30 USD, the Target Boards lower the price threshold for engagement, allowing more system developers to enjoy the benefits of Renesas’ broad-based 32-bit RX MCU Family.

The RX Target Boards provide an inexpensive entry point for embedded designers to evaluate, prototype and develop their products. Each board kit features an on-chip debugger tool that enables application design without requiring further tool investments. Through-hole pin headers provide access to all MCU signals pins, making it easy for customers to interconnect to standard breadboards for fast prototyping.

“What makes the RX Target Board evaluation concept unique is its innovative approach to reusing the same PCB for all MCU variations,” said Tim Burgess, Senior Director, Proprietary MCU Business Division, Renesas Electronics Corporation. “Since each member of the Renesas RX MCU Family has a common pin assignment, customers experience a smooth transition between different RX Groups and RX Series using the same package version. In the case of the RX Target Boards, the widely used 100-pin LQFP package is on board.”

The RX Target Boards offer everything designers need to start board and demo development, including a board circuit diagram and bill of materials, demo source code, user manual, and application notes. Coming soon are additional Target Board variations that will provide full coverage of the entire RX Family, from the low-power RX100 Series to the high-performance RX700 Series.

Key Features of the RX65N MCUs

The RX65N MCU Group combines an enhanced RX CPU core architecture and 120 MHz operation to achieve processing performance of 4.34 CoreMark/MHz. The MCUs include an integrated Trusted Secure IP, enhanced, trusted flash functionality, and a human-machine interface (HMI) for industrial and network control systems operating at the edge of the Industrial Internet of Things (IIoT). The RX65N MCUs also include an embedded TFT controller and integrated 2D graphic accelerator with advanced features ideal for TFT displays designed into IIoT edge devices or system control applications. In addition, the RX65N MCUs include embedded communication-processing peripherals such as Ethernet, USB, CAN, SD host/slave interface, and quad SPI.

Key Features of the RX130 MCUs

The RX130 MCU Group provides 32 MHz operation with flash memory sizes up to 512 KB, and package sizes up to 100-pins to provide higher performance and compatibility with the RX231/RX230 Group of touch MCUs. The ultra-low power, low-cost RX130 Group adds higher responsiveness and functionality for touch-based applications requiring 3V or 5V system control and low power consumption. Featuring a new capacitive touch IP with improved sensitivity and robustness, and a comprehensive device evaluation environment, the new 32-bit RX130 MCUs are an ideal fit for devices designed with challenging, non-traditional touch materials, or required to operate in wet or dirty environments, such as a kitchen, bath, or factory floor.

Key Features of the RX231 MCUs

The RX231 MCU Group operates at 54 MHz and combines a 32-bit RXv2 CPU core with improved DSP/FPU and low-power consumption to realize extreme power efficiency. High-performance digital filtering, floating-point operations, and other processing can be performed even in environments with low-current supply capacity. The RX231 Group includes communication security and encryption functions, and is equipped with capacitive touch sensor capabilities that combine high sensitivity with a high level of noise tolerance, as well as SD host interface, USB, and CAN communication functionality.

Pricing and Availability

The RX Target Boards are available now through Renesas Electronics’ worldwide distributors with a recommended resale price below $30 USD. For more information, please visit: www.renesas.com/rxtb.

(Pricing and availability are subject to change without notice.)

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on