Skip to main content

Renesas Electronics Ships Space Industry's First Radiation-Hardened 100V and 200V GaN FET Power Supply Solutions

ISL70040SEH Low Side GaN FET Driver Powers ISL7002xSEH GaN FETs in Launch Vehicle and Satellite Power Supplies

November 4, 2020

TOKYO, Japan, February 7, 2018 – Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today announced the space industry’s first radiation-hardened, low side Gallium Nitride (GaN) field effect transistor (FET) driver and GaN FETs that enable primary and secondary DC/DC converter power supplies in launch vehicles and satellites, as well as downhole drilling and high reliability industrial applications. These devices power ferrite switch drivers, motor control driver circuits, heater control modules, embedded command modules, 100V and 28V power conditioning, and redundancy switching systems.

The ISL70023SEH 100V, 60A GaN FET and ISL70024SEH 200V, 7.5A GaN FET use the base die manufactured by Efficient Power Conversion Corporation (EPC). The GaN FETs provide up to 10 orders of magnitude better performance than silicon MOSFETs while reducing package size by 50 percent. They also reduce power supply weight and achieve higher power efficiency with less switching power loss. At 5mΩ (RDSON) and 14nC (QG), the ISL70023SEH enables the industry’s best figure of merit (FOM). Both GaN FETs require less heat sinking due to reduced parasitic elements, and their ability to operate at high frequencies allows the use of smaller output filters, which achieve excellent efficiencies in a compact solution size. Manufactured using a MIL-PRF-38535 Class V-like flow, the ISL70023SEH and ISL70024SEH offer guaranteed electrical specifications over the military temperature range and lot-by-lot radiation assurance for high dose rate 100krad(Si) and low dose rate 75krad(Si).

The ISL70040SEH low side GaN FET driver powers the ISL7002xSEH GaN FETs with a regulated 4.5V gate drive voltage and splits the outputs to adjust FET turn-on and turn-off speeds. Operating with a supply voltage of 4.5V to 13.2V, the FET driver provides high current source and sink capability for high frequency operation, while offering both inverting and non-inverting gate drive to provide flexibility in power supply designs. Its fail-safe protection on the logic inputs eliminates unintentional switching when they are not actively driven. The ISL70040SEH provides reliable performance when exposed to total ionizing dose (TID) or heavy ions, and is immune to destructive single event effects (SEE) up to 16.5V with linear energy transfer (LET) of 86MeV•cm2/mg. The GaN FET driver uses a MIL-PRF-38535 Class V manufacturing flow and wafer-by-wafer radiation assurance testing.

“We are pleased to see Renesas Electronics continue Intersil’s six decades of spaceflight product development and leadership,” said Alex Lidow, EPC’s co-founder and CEO. “It is especially gratifying and exciting to see our innovative enhancement-mode gallium nitride-on-silicon (eGaN®) FET technology at work with Renesas’ new radiation-hardened GaN FET driver. These products demonstrate how eGaN technology increases the performance and reduces the cost for applications currently being served by MOSFETs.”

“Size, weight and power efficiency mean everything to designers and manufactures of launch vehicles and satellites,” said Philip Chesley, Vice President of Industrial Analog and Power Business Division, Renesas Electronics Corporation. “The new ISL7002xSEH GaN FETs and ISL70040SEH GaN FET driver represent the most meaningful power management innovation we’ve seen in a long time for the spaceflight industry.”

Key Features of ISL70023SEH and ISL70024SEH GaN FETs

  • Very low RDSON at 5mΩ (typ) - ISL70023SEH; and 45mΩ (typ) - ISL70024SEH
  • Ultra-low total gate charge 14nC (typ) - ISL70023SEH; and 2.5nC (typ) - ISL70024SEH
  • Radiation hardness assurance (lot-by-lot):
    • High Dose Rate (HDR) (50-300rad(Si)/s):100krad(Si)
    • Low Lose Rate (LDR) (0.01rad(Si)/s): 75krad(Si)
  • SEE hardness at LET 86MeV•cm2/mg
    • ISL70023SEH, VDS = 100V, VGS = 0V
    • ISL70024SEH, VDS = 160V, VGS = 0V
  • Full military temperature range operation
    • TA = -55°C to +125°C
    • TJ = -55°C to +150°C

Key Features of ISL70040SEH GaN FET Driver

  • Wide operating voltage range from 4.5V to 13.2V
  • Up to 14.7V logic inputs (regardless of VDD level), inverting and non-inverting inputs
  • Full military temperature range operation
    • TA = -55°C to +125°C
    • TJ = -55°C to +150°C
  • Radiation hardness assurance (wafer-by-wafer):
    • High Dose Rate (HDR) (50-300rad(Si)/s):100krad(Si)
    • Low Lose Rate (LDR) (0.01rad(Si)/s): 75krad(Si)
  • SEE hardness at LET = 86MeV•cm2/mg:
    • no SEB/SEL, VDD = 16.5V
    • no static input SET, VDD = 4.5V and VDD = 13.2V
  • Electrically screened to DLA SMD 5962-17233

The ISL70023SEH 100V, 60A GaN FET or ISL70024SEH 200V, 7.5A GaN FET can be combined with the ISL70040SEH low side GaN FET driver and the ISL78845ASEH PWM controller to create launch vehicle and satellite switched mode power supplies.

Availability

The rad-hard ISL70023SEH 100V, 60A GaN FET and ISL70024SEH 200V, 7.5A GaN FET are available now in hermetically sealed 4-lead 9.0mm x 4.7mm SMD packages. For more information on the ISL70023SEH, please visit: www.intersil.com/products/isl70023seh. For more information on the ISL70024SEH, please visit: www.intersil.com/products/isl70024seh.

The rad-hard ISL70040SEH low side GaN FET driver is available now in a hermetically sealed 8-lead 6mm x 6mm SMD package. For more information on the ISL70040SEH, please visit: www.intersil.com/products/isl70040seh.

(Note) Renesas branding policy will continue to apply the Intersil brand for military and aerospace products.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) eGaN is a registered trademark of Efficient Power Conversion Corporation (EPC). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on