TOKYO, Japan, November 16, 2016 – Renesas Electronics Corporation, a premier provider of advanced semiconductor solutions, today announced its latest innovative developments in Ethernet time-sensitive networking (TSN). Renesas has become the world’s first to demonstrate standard compliance and interoperability for frame preemption, the most essential feature for TSN (Note 1) at the AVnu Plugfest (Note 2).
Ethernet TSN standards are currently under development by the TSN task group of IEEE802.1. Their goal is to pave the way for seamless deterministic communication via Ethernet for automotive in-vehicle networking and within the industrial internet.
Recently, the extension of the Ethernet AVB (Audio Video Bridging) standards for professional audio and in-vehicle networks, etc. is progressing. The standards cover several features, including time synchronization as well as traffic scheduling, frame preemption and ingress policing. With these features, the TSN technology is expected to accelerate the harmonization of Ethernet technologies in Industry 4.0 applications as well as in the automotive market, such as for high-speed in-vehicle networks.
Renesas has developed two TSN demonstrations for automotive and industrial networking to illustrate the potential benefits of the TSN standard. The demonstrations will be showcased at the upcoming Automotive Networks to be held on November 17 in Munich, Germany, and SPS IPC Drives exhibitions, to be held from November 22 to November 24 in Nuremberg, Germany.
Renesas’ TSN engagement for automotive
Renesas offers a variety of semiconductor solutions that support Ethernet AVB, which is already widely used in automotive networks. Building on its expertise in in-vehicle communication technology, Renesas has become the world’s first to demonstrate standard compliance for frame preemption as first in the industry. Renesas will showcase the new TSN demonstration at the upcoming Automotive Networks event in Munich on November 17, 2016. Renesas will also provide more details about the company’s TSN switch solution adapted to the upcoming IEEE 802.1 standards. The TSN technology is expected to realize wider use of Ethernet for in-vehicle networks and even replace the previous networks used for critical control. Renesas is also eyeing the possible replacement of the existing Ethernet with the TSN for automotive control systems, and intends to promote TSN standard in automotive networks to contribute to the realization of more suitable and safer autonomous-driving vehicles.
Renesas TSN engagement for Industry 4.0
With its rich lineup of industrial network solutions that support a variety of industrial Ethernet standards, Renesas is contributing towards the realization of Industry 4.0. The latest generation of industrial Ethernet standards often come with proprietary layer-2 implementations, which make network convergence difficult. The consequences are isolated networks that require gateways to be connected to other hierarchies. Renesas is working to combine the current generation of industrial network technology with TSN to make it future-proof while also supporting legacy standards by offering best-in-class solutions.
Renesas will showcase the TSN demonstration on stand 142, Hall 6 at the upcoming SPS IPC Drives fair 2016 in Nuremberg.
Renesas TSN demonstrations features
The TSN demonstration for automotive application is based on a future in vehicles network domain architecture. It shows tunneling of CAN traffic via Ethernet and the effects of various TSN features that can be enabled or disabled on demand.
The TSN demonstration for industrial applications is designed with the factory network in mind where various devices are connected. This demonstration showcases the effects of TSN features on motor control for which real time control is essential, on a network where traffic from various devices coexists.
Main features of TSN standard shown in the demonstration
Along with many standard switch features, the TSN demonstrations will specifically include the following features:
- Forwarding and Queuing Enhancements for Time-Sensitive Streams. (IEEE 802.1Qav)
This is an mechanism to shape the traffic by establishing a fairness transmission of priority traffic by reservation of limited bandwidth per traffic class; this is also known as “Credit-Based Shaping” - Enhancements for Scheduled Traffic (IEEE 802.1Qbv)
With this feature, the traffic can be classified to one of the eight traffic classes, and the classes can then be scheduled to allow for them to communicate at a fixed repetitive cycle. - Timing and Synchronization (IEEE 1588v2 / IEEE 802.1AS)
This is the classic master-slave protocol to synchronize the clocks between the network participants - Frame Preemption/Interspersing Express Traffic (IEEE 802.1Qbu/802.3br)
A new mechanism that allows a time-critical frame to interrupt a non-time-critical frame in order to reduce latency. Renesas is one of the few companies joined the first AVnu Plug Fest (Note 2) held in August 2016 at the University of New Hampshire’s Interoperability Laboratory (UNH-IOL). The event focused on Frame Preemption/Interspersing Express Traffic, and there the strict compliance and interconnectivity of Renesas technology had been confirmed.
Renesas intends to continue to support promotion of the Ethernet TSN standard and its adoption in the automotive and industrial fields to contribute to the development of autonomous-driving vehicles and Industry 4.0.
(Note 1) Renesas demonstrated during the AVnu Plugfest devoted to presentations of frame preemption/interspersing express traffic that was held for the first time in August 2016.
(Note 2) A connectivity testing event sponsored by AVnu Alliance, the body responsible for defining Ethernet TSN connectivity specifications, and implemented by the University of New Hampshire's Interoperability Laboratory (UNH-IOL), the official certification organization for Ethernet TSN.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks) All other registered trademarks or trademarks are the property of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.