Skip to main content

Renesas Expands Communication Timing Portfolio for 4G/5G Radio

Strong Lineup Delivers Best-in-Class Phase Noise, Industry’s First Complete 5G Radio Synchronization Solution

March 23, 2021

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today expanded its communication timing portfolio with three new low phase noise, high-frequency RF timing solutions for 4G and 5G radio, and two new Winning Combinations to address the need for full signal chain solutions. The new 8V19N850 radio synchronizer and 8V19N880, 8V19N882 JESD204B/C clock jitter attenuators deliver ITU-T compliant network clock synchronization, best-in-class phase noise, and high clock frequency.

“Network synchronization plays an increasingly crucial role in the transition to 5G,” said Bobby Matinpour, Vice President of Timing Products, Data Center Business Division at Renesas. “With these latest devices and our new Winning Combinations, we enable our communications customers to introduce next-generation solutions with superior performance and reliability.”

The 8V19N850 radio synchronizer is the industry’s first integrated 5G radio synchronization solution and is equipped with a complete set of features for radio synchronization on a single chip; including full ITU-T G.8273.2 T-BC/T-TSC Class C, ITU-T G.8262.1 enhanced SyncE, and JESD204B/C compliance. The 8V19N850 also takes care of recovering the clock from CPRI/eCPRI, per IEEE 802.1cm fronthaul synchronization requirements, making it ideally suited for use in emerging 5G O-RAN networks for Radio Units (O-RU).

The 8V19N880 and 8V19N882 JESD204B/C clock jitter attenuators deliver low phase noise and exceptional jitter performance as low as 74fs RMS and -90dB spurious attenuation for mission-critical industrial data converter applications in wireless radio, test & measurement, instrumentation, and high-performance imaging. The new devices support frequencies up to 3932.16 MHz (up to 6 GHz with an external VCO) and feature 16 and 18 integrated differential outputs to deliver a first-in-class balance of high performance, low voltage, and low power consumption with 1.8V support.

The devices are also featured in Renesas’ two new Winning Combinations, designed to address increasing demand for higher bandwidth for cellular services. The Small Cell Radio and MIMO Radio solutions use mutually compatible devices for lower risk and faster time to market. They also showcase the combined benefits of the new RF timing ICs paired with Renesas’ complementary microcontroller and power management offerings to accelerate solution design.

As the market leader in silicon timing, Renesas offers the only “one-stop-shop” for timing solutions, offering expertise and products from full-featured system solutions to simple clock building-block devices.

Availability

The new 8V19N850, 8V19N880 and 8V19N882 RF timing ICs are available now. For more information, please visit renesas.com/radiosynchronizers.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on