TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today expanded its family of 8.2mm creepage photocouplers with three new devices designed for operation in harsh industrial automation equipment, solar inverter, and EV charger operating environments. Measuring a mere 2.5mm x 2.1mm in an LSSO5 package, the world’s smallest optical isolated IGBT drivers and intelligent power module (IPM) driver reduce PCB mounting areas by up to 35 percent compared with other devices on the market.
“Industrial equipment and green energy system manufacturers are currently facing two core challenges: Equipment needs to get smaller, requiring downsizing for factory floor efficiency and higher functionality equipment within the same board size, while at the same time, safety standards are getting stricter,” said Philip Chesley, Vice President, Industrial and Communications Business Division at Renesas. “Our expanded portfolio of small isolation devices offers customers greater layout flexibility with more options to enable longer secured creepage distance for high-voltage inverter control applications.”
The new RV1S9231A 2.5A output and RV1S9207A 0.6A output IGBT drivers and RV1S9209A active high output IPM driver come in low-profile LSSO5 packages with a 0.65mm pin pitch, deliver 5,000 Vrms isolation voltage, and support high temperature operation up to 125°C to withstand the harsh operating environments. The photocoupler trio also supports 200V and 400V systems with reinforced insulation to meet stringent industrial safety standards, adhering to the strict UL61800-5-1 standards for motor drive equipment.
Renesas has identified and created a system architecture for various applications where the RV1S92xxA family of products adds tangible value in the system. For instance, a new AC Drives / GP Inverters “Winning Combination” featuring the RV1S92xxA family of products enables customers to downsize their industrial equipment and inverter systems that meet UL61800-5-1 standard. Renesas’ Winning Combinations are vetted system architectures made from mutually compatible devices that work together seamlessly. Renesas offers over 200 Winning Combinations for a wide range of applications and end products which can be found at renesas.com/win.
Availability
The RV1S9209A, RV1S9231A, and RV1S9207A photocouplers are available now from Renesas’ worldwide distributors. For more information on the broad optoelectronic portfolio, please visit: renesas.com/photocouplers.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.