WattShare Technology Transforms Consumer, Industrial, and Medical Mobile Devices into Wireless Charging Hubs

September 8, 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, introduced the P9415-R wireless power receiver with Renesas’ exclusive WattShare™ technology as the newest member of its wireless power solutions portfolio. The new 15W wireless power receiver enables smartphones, power banks, and portable industrial and medical equipment, to wirelessly charge other mobile devices and accessories that also have wireless charging capabilities. The P9415-R features up to 5W of transmit power capability in transmitter/receiver (TRx) mode, as well as receive up to 15W on Qi transmitters, enabling quick and convenient mobile device charging on the go.

“2020 will be the year wireless charging moves into the mainstream, expanding from premium smartphones to include mid-range devices, and gaining broader adoption into consumer and industrial devices beyond the smartphone market,” said Andrew Cowell, Vice President, Mobility, Infrastructure & IoT Power Business Division at Renesas. “With the P9415-R, we are excited to bring our state-of-the-art WattShare technology to a wider audience, offering customers broader access to robust, scalable and flexible solutions that enable quick, convenient, and cost-effective wireless charging for portable devices.”

Based on Renesas’ proprietary WattShare technology, the P9415-R combines receiver and transmitter capabilities, allowing smartphones, smartwatches, truly wireless ear buds and other devices to be wirelessly charged simply by placing them on top of a smartphone or other industrial and medical portable devices. In WattShare TRx mode, the P9415-R enables these mobile devices to change the power flow direction and deliver up to 5W of power to charge other devices. Customers can use the same wireless power coil and same P9415 circuitry to both receive and transmit power wirelessly.

Key Features of P9415-R Wireless Power Receiver

  • MTP non-volatile memory for easy firmware and device function updates
  • GUI support offering greater flexibility for user customization
  • Receives up to 30W in proprietary mode
  • UVLO as low as 2.7V for increased available charging area and fast connections
  • Improved IOUT sensing accuracy for improved foreign object detection capabilities
  • Supports an easier path to QI certification and speeds time to market
  • Bi-directional communications to support proprietary authentication with encryption
  • X-Y alignment circuitry for better receiver/transmitter device alignment
  • WPC 1.3 ready – Renesas’ first WPC 1.3-ready wireless power receiver

Renesas is the global leader in wireless power solutions for both the Power Receivers (PRx) used in smartphones and other applications, as well as the Power Transmitters (PTx) used in charging pads and automotive in-car applications. Visit https://www.idt.com/wirelesspower to learn more about Renesas’ wireless power solutions.

Availability

The P9415-R 15W WattShare wireless power receiver is available now. For more information, please visit www.idt.com/P9415R.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power,and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future.Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) WattShare is a trademark of Renesas Electronics Corporation. All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on