TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today expanded its popular ZMOD4410 Indoor Air Quality (IAQ) sensor platform with the industry’s first software-configurable IP67-qualified waterproof option for IAQ applications operating in wet or dirty environments such as kitchens, bathrooms, and hospital rooms, where they are frequently exposed to water, oils, and dust.
The firmware-configurable waterproof ZMOD4410 sensor features a unique hermetically sealed package that protects the sensor from water and dust with a hydrophobic and oleophobic material that is permeable to humidity and volatile organic compounds (VOCs) at the same time. By combining IP67-rated packaging with the industry-leading accuracy and reliability that the ZMOD4410 platform is known for, Renesas enables new, low-power IAQ applications that operate in splash zones, while maintaining the high precision and flexibility customers need to customize their systems and eliminating the need for expensive waterproofing systems.
“The increasing use of IAQ sensors in splash zone environments along with other areas with frequent exposure to water, oils, and dust drives higher demand for protection from those elements without sacrificing performance – a traditionally expensive process that requires additional hardware and firmware,” said Uwe Guenther, Senior Director, Sensing Solutions, IoT and Infrastructure Business Unit at Renesas. “The new waterproof ZMOD4410 sensor combines the best of both worlds cost effectively, enabling broader adoption of highly accurate smart sensing devices that can operate in high-humidity and harsh conditions for a wider range of market applications.”
Key Features of the Waterproof ZMOD4410 Sensor
The IP67-rated ZMOD4410 sensor maintains superior accuracy and high performance while eliminating the need for expensive waterproofing systems, making it ideal for use in waterproof end use applications. The sensor is shipped fully calibrated in the hydrophobic and oleophobic package, and customers can apply a conformal coating on their circuitry rather than adding an external membrane to the module. As part of the ZMOD4410 family, the waterproof sensor features AI firmware implemented on an MCU to improve sensing performance, and is also highly resistant to siloxanes, enabling exceptional reliability for use in harsh applications.
Renesas’ unique software-configurable ZMOD platform provides greater design flexibility for smart sensing systems, allowing firmware updates in the field that enable new, application-specific capabilities such as selective measurements to detect VOCs. This includes IAQ measurement within international guidelines, allowing customers to measure total VOCs (TVOCs) in the low parts-per-million range (ppm). The higher accuracy and consistency provides improved estimated Carbon Dioxide (eCO2) levels. The new waterproof ZMOD4410 sensor module supports all firmware updates to date.
The combination of water proofing, reliability, programmability, best-in-class stability, and sensitivity in measuring VOCs makes the new waterproof sensor an ideal solution for IAQ devices, including smart HVAC systems, ventilator fans, bathroom lights and switches, and wearables, that operate in a wide range of high-humidity, splash zone, dirty, or submersible environments.
Availability
The ZMOD4410 sensor with hydrophobic package is available now. For more information, please visit www.renesas.com/zmod4410.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.