High-Speed, Low-Power Data Buffer Delivers Improved Speed and Bandwidth for DDR5 DRAM and Storage Class Memory Modules
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions and the industry leader in memory interface products, today announced a new high-speed, low-power DDR5 data buffer for data center, server, and high-performance workstation applications.
Advancements over the past few years in real-time analytics, machine learning, HPC, AI, and other memory and bandwidth-hungry applications have fueled explosive growth in server memory bandwidth requirements. The new JEDEC-compliant DDR5 data buffer 5DB0148 from Renesas enables significantly higher speeds and lower latency for load-reduced dual inline memory modules (LRDIMMs) that have become the cornerstone memory technology for this new class of applications. The first generation of DDR5 LRDIMMs based on Renesas components enable a bandwidth increase of more than 35 percent over DDR4 LRDIMMs operating at 3200 MT/s.
“As the industry’s complete DDR5 solution provider, we are working closely with customers and ecosystem partners to launch a vastly expanded portfolio of memory solutions into production,” said Rami Sethi, Vice President, Data Center Business Division at Renesas. “Our DDR5 data buffers are critical to enabling high performance DRAM solutions such as LRDIMMs, alternative high density modules and heterogeneous memory solutions, all of which empower a new generation of high performance computing applications.”
The Renesas DDR5 Data Buffer maximizes channel eye opening for systems that are heavily loaded through a combination of capacitive load reduction, data alignment, and signal recovery techniques. This allows server motherboards with a large number of memory channels and slots and complex routing topologies to run at maximum speed, even when fully populated with high-density memory. Additionally, improvements in the DDR5 modules definition allow for lower power supply voltages (1.1V vs 1.2V in DDR4), on-DIMM voltage regulation, and implementation of advanced control plane architectures with the use of the SPD Hub and modern control bus communications such as I3C.
Renesas is the longest running supplier of memory interface products in the industry with a history of developing complete chipset solutions since the inception of dual inline memory modules. As part of a complete family of solutions, the new Renesas DDR5 data buffer 5DB0148 is optimized to work seamlessly with the other DDR5 Renesas components on an LRDIMM memory module, including the power management IC P8900, the registered clock driver 5RCD0148, the SPD Hub SPD5118, and the temperature sensor TS5111. Memory vendors deploying Renesas chipset solutions are assured of full interoperability and robust quality.
Availability
The DDR5 data buffer 5DB0148 is sampling to qualified customers. For additional information, visit www.idt.com/5db0148.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.