Skip to main content

Renesas Introduces Rugged and High Performance 100V Half-Bridge MOSFET Drivers

Robust HIP221x Drivers Combine High Speed and High Voltage to Extend Renesas’ 25-Year MOSFET Driver Legacy in Industrial and Consumer Applications

November 4, 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced the HIP2211 and HIP2210, a new pair of 100V half-bridge MOSFET drivers. The HIP2211 is a next-generation pin-compatible upgrade to Renesas’ popular ISL2111 bridge driver, while the new HIP2210 offers a tri-level PWM input to simplify power supply and motor drive design. The HIP2211 and HIP2210 are ideal for 48V telecom power supplies, Class-D audio amplifiers, solar inverters, and UPS inverters. They are also rugged enough to power the demanding 48V motor drives found in Li-ion battery-powered household and outdoor products, water pumps, and cooling fans.

The HIP221x drivers are designed to work reliably under difficult operating conditions, with the high-speed, high-voltage HS pin tolerating up to -10V continuously and slewing as quickly as 50V/ns. Comprehensive under-voltage protection works in tandem with the HIP2210’s programmable anti-shoot-through protection to ensure the driven MOSFETs are not damaged due to power supply or other external fault conditions. Renesas’ HIP221x drivers feature strong 3A source, 4A sink drivers with very fast 15ns typical propagation delay and 2ns typical delay matching, making them the optimal solution for high-frequency switching applications. Both the HIP2210 and HIP2211 are designed to complement Renesas microcontrollers in advanced DC/DC and brushless motor drive systems.

“The innovative HIP221x devices continue our 25-year heritage of developing industry leading Harris Intelligent Power (HIP) half-bridge drivers, said Philip Chesley, Vice President, Industrial and Communications Business Division at Renesas. “Robust noise tolerance, ultra-fast propagation delays, and high system efficiency are some of the key features our customers have come to rely on from our entire range of HIP half-bridge MOSFET drivers.”

Key Features of HIP2211 and HIP2210

  • 115VDC bootstrap supply maximum voltage (120V HS absolute maximum) supports 100V on the half-bridge
  • Wide VDD voltage operating range of 6V to 18V (20V absolute maximum)
  • HS pin tolerates up to -10V and 50V/ns slew rates
  • Integrated 0.5Ω typical bootstrap diode eliminates external discrete diodes
  • VDD and boot UVLO prevent low gate voltage drive to the NFETs
  • Adjustable dead time delay via RDT pin (HIP2210 only) prevents shoot-through conditions, adjustable from 35ns to 350ns with a single resistor

Pricing and Availability

The HIP2211 and HIP2210 are available now from Renesas’ worldwide distributors, both priced at $1.30 USD in 1,000-unit quantities. The HIP2211 is supplied in an 8-lead SOIC and a 10-lead 4mm x 4mm TDFN package. For more information and evaluation board, please visit: www.renesas.com/products/hip2211.

The HIP2210 is supplied in a 10-lead 4mm x 4mm TDFN package. For more information and evaluation board, please visit: www.renesas.com/products/hip2210.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks). All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on