Quick-Connect IoT System Combines Modular and Standardized Hardware and Software Building Blocks for MCUs and Sensors; Solidifies Renesas’ IoT Leadership
TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced an innovative new IoT system design platform that significantly eases the prototyping of IoT systems. The Renesas Quick-Connect IoT system consists of standardized boards and interfaces, enabling designers to quickly and easily connect a wide range of sensors to MCU development boards. The new system also delivers core software building blocks that are portable between boards, greatly reducing coding requirements.
As part of the Quick-Connect IoT system, Renesas has worked with Digilent, Inc. in creating a new expanded I2C Pmod Interface, Type 6A, for wider coverage and added flexibility. Renesas has standardized on the new Pmod 6A connector from Digilent for new sensor Pmods and MCU development kits. This standardization allows designers unmatched flexibility in selecting the optimal combination for any IoT prototype design. MCU boards will have two Pmod connectors, one for a sensor Pmod, and another for a communications module. The Pmods can also be cascaded for even greater flexibility.
Renesas has also redefined common software APIs (Application Program Interfaces) and HAL (Hardware Abstraction Layer) code for a wide variety of sensors. These are embedded into the Renesas e2 studio integrated development environment. Now, instead of writing and testing hundreds of lines of driver code, designers only need to graphically select their sensor and write a few lines of code. All the integration and setup effort is taken care of behind the scenes, reducing the time to a working solution.
“We are laser focused on delivering solutions that enable customers to get to market faster with superior end products,” said DK Singh, Senior Director of the Systems and Solutions Team at Renesas. “For example, we’ve developed hundreds of Winning Combinations that give an our customers an elevated design platform to mitigate the design risks and reduce development time. Quick-Connect IoT is the latest example of our commitment in this area and we will expand its coverage to support more boards and devices in the future. Additionally, having a standardized hardware connectivity platform allows customers to use compatible Pmods developed by third parties and other suppliers.”
“The new Pmod interface Type 6A manifests our vision of making system prototyping easier and more accessible,” said Talesa Bleything, Director of Marketing at Digilent, Inc. “It conforms to the I2C specifications with an optional interrupt and reset pin plus optional control signals, giving users added flexibility for diverse types of system development.”
Initially, Quick-Connect IoT will include over a dozen new Renesas sensor Pmods and other modular boards, including air quality sensors, flow sensors, bio-sensing, time of flight, temperature and other sensing elements. Additional Renesas sensor Pmods are under development that will include a variety of sensors and peripherals. Over 25 MCU development boards and kits spanning the RA, RX and RL78 families are compatible with the new Pmod Type 6A standard, either directly or through a small interposer board developed by Renesas. RE and RZ development boards will be supported in the near future. Customers can order development kits, sensor and interposer boards through Renesas sales and sample channels.
“Our IoT customers require more than great MCUs, sensors and software,” said Chris Allexandre, Senior Vice President of Sales and Digital Marketing, IoT and Infrastructure Business Unit at Renesas. “Quick-Connect IoT is a game-changer that extends our leadership in the IoT market.”
Availability and More Information
The Quick-Connect IoT design system is available today through a wide range of hardware and software offerings from Renesas. For a list of available boards, links to software downloads, literature, how-to videos and more, customers can visit www.renesas.com/quickconnect.
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.