Skip to main content

Renesas Unveils Integrated LIN Interface Sensor Signal Conditioner for Electric and Hybrid Electric Vehicle HVAC Systems

ZSSC4132 Delivers High Accuracy, Flexibility, and High Cost Efficiency with Integrated LIN, Best-in-Class Analog Front End, and Reduced Bill of Materials

July 9, 2020

TOKYO, Japan ― Renesas Electronics Corporation (TSE:6723), a premier supplier of advanced semiconductor solutions, today introduced the ZSSC4132 – an automotive pressure sensor solution featuring an integrated certified LIN v2.2a interface. The single-package sensor signal conditioner (SSC) delivers best-in-class performance, increased design flexibility, and cost efficiency in a compact form factor for HVAC applications used in plug-in hybrid electric vehicle (PHEV), Battery Electric Vehicle (BEV), and Fuel-cell Electric Vehicle (FCEV) climate control systems.

The ZSSC4132 can be configured for nearly all resistive bridge sensors. This flexibility, combined with leading performance levels, an integrated LIN PHY, small package footprint, and AEC-Q100 Grade 0 qualifications, makes the SSC ideally suited for small automotive sensor modules with limited space, tight budget and end-of-line (EOL) calibration requirements.

“HVAC plays a significant role in EV battery range, and OEMs are looking for ways to improve system efficiency while maintaining high performance and staying within tight cost constraints,” said Christian Wolf, Vice President, Automotive Sensor Business Division at Renesas. “With the ZSSC4132, customers can access a complete SSC solution that is already LIN certified, allowing them to easily and cost effectively scale their HVAC system development for mid-range up to high-end EVs and HEVs.”

Key Features of the ZSSC4132

The ZSSC4132 combines best-in-class analog front end (AFE) technology for enhanced sensor signal conditioning as well as digital calibration to significantly reduce the noise sensitivity and deliver high accuracy for pressure and temperature readings. The SSC’s integration reduces overall bill of material (BOM) requirements by minimizing the need for external components. In addition, the ZSSC4132’s unique digital calibration feature that allows customers to minimize calibration efforts, further reducing overall system costs.

Additional features include:

  • LIN v2.2a certification with backwards compatibility to LIN v1.3, v2.0, and v2.1
  • Differential bridge sensor input that enables accuracy at ±0.5% full scale output for temperatures ranging from -40°C to 150°C
  • 12- to 14-bit ADC resolution
  • Slave node position detection feature at the LIN bus, allowing the SSC to assign a unique ID to the device
  • Overvoltage and reverse-polarity protection circuitry
  • Electromagnetic compatibility
  • Multiple diagnostic features

Availability

The ZSSC4132 is available now in a 4mm x 4mm, 24-lead QFN package with prices starting at $1.38 USD per unit in 10,000-unit quantities. An evaluation kit for the ZSSC4132 is also available now with prices starting at $185 USD.

For more information on the ZSSC4132 SSC, including technical documentation and tools, please visit https://www.idt.com/zssc4132.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All names of products or services mentioned in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on