Innovation
Renesas’ Strategy for Sustainable Technology
Automotive, Infrastructure and Industrial IoT industries have experienced rapid changes in recent years, such as Connected, Autonomous, Shared & Services, Electric (CASE) vehicles and Digital Transformation (DX). In addition, the ongoing COVID-19 pandemic has significantly changed our lifestyles, accelerating a paradigm shift globally.
At Renesas, one of our core businesses provides products and innovation that contribute to a sustainable society and sectors that are critical to people’s work and daily lives, such as automotive, factory automation (FA), communication infrastructure, medical care, and healthcare. Specifically, Renesas invests in product development and technological innovation with a focus on the power efficient solutions and other solutions that make people’s lives safe and secure. We have also defined our four core technologies to support our sustainable products and solutions. We have developed and implemented an action plan including periodic reporting to the board, evaluation, and corrective actions.
To this end, Renesas invested a total of 220 billion yen (non-GAPP basis, equivalent to approximately 15% of total sales) in research and development in 2023. In order to strengthen our existing business and advance technological capabilities, we plan to make the same level of investment in research and development in coming years.
Renesas’ Technological Innovation
Renesas has identified four key technologies: Artificial Intelligence (AI), Safety & Security, Digital & Analog & Power Solution, and Cloud Native.

- Artificial Intelligence (AI): AI is an important technology for enhancing computing power to meet the emerging social needs of an automated, data-centric world.
- Safety & Security: It is the foundation of mission-critical applications that realize a safe and secure society.
- Digital & Analog & Power Solution: As automation and IoT advance various sensor technologies and human interfaces, Digital & Analog & Power Solution enable more optimized and integrated implementations in which the brain (digital) controls the nerves (analog).
- Cloud Native: It is a technology that uses low-latency real-time control and communication to facilitate cloud services on the end-point devices. Embedded systems become valuable by connecting to the cloud and running cloud services.
Artificial Intelligence (AI)
Renesas was one of the first semiconductor suppliers to introduce flexible, scalable embedded artificial intelligence (e-AI) into the end-point devices. We are providing intelligence to the end-point devices in order to realize a safe and secure lifestyle and an environmentally friendly smart society.
Energy-Efficient Computing with AI
Renesas is a proven provider of energy-efficient AI computing solutions for automotive and industrial applications.
Our company also provides DRP-AI Translator, a dedicated development tool that simplifies the implementation of learned AI models. Examples of AI applications based on object recognition include smart shopping cart systems that perform automatic tabulation, industrial robots to work safely with humans, and medical cameras that support physician diagnosis.
Click here to learn more about Renesas' AI technology.
Safety & Security
Renesas meets the growing need for safety and security in connected products. Our company's safety and security technologies are designed to meet the industry's highest ISO/IEC reliability and performance standards, providing solutions that help our customers feel more secure in a world where everything is virtual.
Building "Root of Trust" with Safety and Security Technologies
With 1 billion connected devices worldwide and growing demand for services, there is a huge demand for robust safety and security. From road, car, home safety, and product from manufacturing to consumption, connected devices improve the way we work and live by providing valuable measurement data. Our company uses safety and security technologies to ensure the integrity and confidentiality of systems and data and to reduce the risk of breakdowns and cybersecurity. We provide comprehensive functional safety and security support for mission-critical applications to help our customers build robust systems.
Click here for Renesas' safety technology.
Click here for Renesas' security technology.
As one of the world's leading automotive semiconductor suppliers, our company has actively participated in the ISO 26262 and ISO/SAE 21434 working groups and led the development of functional safety and security technologies for automotive systems. Leveraging our automobile-related experience and core competencies, we are actively proposing new system solutions that can meet our customers' functional safety and security needs.
Digital & Analog & Power Solution
Renesas offers an attractive solution that maximizes system efficiency and performance while reducing power consumption, number of components, and BOM costs through the synergy of its complementary product portfolio of analog + power + embedded processing. These comprehensive systems solutions reduce your time to design and commercialize and ultimately contribute to sustainable development and reduced environmental impact worldwide.
Easy-to-Use, One-Stop Solutions
Renesas Lab on the Cloud
A new solution, Lab on the Cloud, gives customers quick access to Renesas solutions before they receive a real board or start designing. Customers can remotely use an assessment board via an intuitive GUI to assess in real time without the location and time constraints of the past.
This new development environment enables customers to access and test Renesas' proven evaluation boards, winning combinations and software solutions online.
Cloud Native
Cloud Native technology enables cloud services to run smoothly on endpoint devices. To enable Cloud Native embedded devices, system solutions must incorporate advanced software and IT technologies. Renesas is working with cloud providers in a variety of industries to develop cloud-specific core technologies such as safety, security, connectivity, and human machine interface (HMI), and is working on partnerships to do so.
Innovation through Collaboration
Renesas provides a variety of embedded systems and IoT cloud solutions in collaboration with cloud service partners. The published source code includes a middleware stack that supports secure connections with major cloud providers such as Amazon Web Services (AWS), Microsoft Azure, Google Cloud Platform and third-party MQTT brokers. Our company will continue to work closely with its cloud services partners to provide optimal solutions for your systems.
Renesas Partner Program and Consortium
Renesas offers two partner programs: the hardware-focused Renesas Preferred Partner Program and the software-focused Renesas Ready Partner Network. Renesas offers system and solution partners in a number of genres that make Renesas products ideal for use. We also have consortia that specialize in specific fields, such as automotive and industrial sectors.
Please visit respective product websites to learn more about our company's partner programs and consortium activities.
Active Participation in the Open-Source Software (OSS) Community
The Linux Foundation is a non-profit consortium dedicated to promoting Linux growth and collaborating on OSS. Our company has long been a gold member of the Linux Foundation, contributing to open-source development. Renesas is also a Platinum member of the Automotive Grade Linux (AGL) and Civil Infrastructure Platform (CIP) projects.
Renesas’ contributions to the Linux Foundation not only help customers quickly set up community OSS assets, but also help them find highly-skilled engineers from local suppliers. Through the Linux Foundation, our company is committed to sharing innovation and working with the broader community to continue its efforts to ensure the trust and security of OSS for engineers around the world.
Innovation Focus 1 (ISSCC 2024)
Memory Technology:
"A 22nm 10.8Mb Embedded STT-MRAM Macro Achieving over 200MHz Random Read Access and 10.4MB/s Write Throughput with In-field Programmable 0.3Mb MTJ-OTP for High-end MCUs"
(Tomoya Ogawa, Ken Matsubara, Yasuhiko Taito, Tomoya Saito, Masayuki Izuna, Koichi Takeda, Yoshinobu Kaneda, Takahiro Shimoi, Hidenori Mitani, Takashi Ito, Takashi Kono, Renesas Electronics, Tokyo, Japan)
AI Technology:
"A 23.9 TOPS/W @ 0.8V, 130 TOPS AI accelerator with 16x performance accelerable pruning in 14nm heterogeneous embedded MPU for real-time robot applications"
(Koichi Nose, Taro Fujii, Katsumi Togawa, Shunsuke Okumura, Kentaro Mikami, Daichi Hayashi, Teruhito Tanaka, Takao Toi, Renesas Electronics, Tokyo, Japan)
Innovation Focus 2 (ISES JAPAN 2024 Keynote Speech)
Shinichi Yoshioka, Co-CTO of Renesas, was invited to speak at the International Semiconductor Executive Summit Japan (ISES JAPAN, March 6, 2024), an international conference that brings together leading semiconductor manufacturers, equipment and material suppliers, and research institutes to discuss innovative technologies.
In his speech, Renesas emphasized the importance of promoting the cooperative design of hardware and software, as well as the key points of chiplet development as an area to implement and advance this concept.
The pursuit of Digitalization/Virtualization as an innovative technology that makes it easier for customers to develop systems remains a major guiding principle for Renesas.
Contributing to SDGs
The Renesas Group's innovation initiatives contribute to the following Sustainable Development Goals.

SDG 9.5 "Promote scientific research and enhance technical capacity in the industrial sector in all countries, including developing countries, by promoting innovation by 2030, substantially increasing the number of R&D workers per 1 million people, and increasing public and private R&D spending."