Basic Library
Digital I/O
Analog I/O
Advanced I/O
Time
Math
Trigonometry
Random Numbers
Bits and Bytes
Interrupts
Communication
Standard Library
Servo Motor
Stepper
Liquid Crystal
EEPROM
SPI
I2C (Wire)
SD Card
SD Card (File Control)
Ethernet
Ethernet (Server)
Ethernet (Client)
Firmata
Periodic Operation
Power Save
Clock (RTC)
SoftwareSerial
Utility
Math
This library allows for the calculation of min/max, absolute value and the square root of a number. Users can also constrain a number within a range, re-map a number from one range to another, and calculate the value of a number raised to a power.
min
Description
Calculates the minimum of two numbers.
Syntax
min(x, y)
Parameters
x: The first number, any data type
y: The second number, any data typeReturns
The smaller of the two numbers.
max
Description
Calculates the maximum of two numbers.
Syntax
max(x, y)
Parameters
x: The first number, any data type
y: The second number, any data typeReturns
The larger of the two parameter values.
abs
Description
Computes the absolute value of a number.
Syntax
abs(x)
Parameters
x: The number
Returns
If x is greater than or equal to 0. -x: If x is less than 0.
constrain
Description
Constrains a number to be within a range.
Syntax
constrain(x, a, b)
Parameters
x: The number to constrain, all data types
a: The lower end of the range, all data types
b: The upper end of the range, all data typesReturns
x: If x is between a and b. a: If x is less than a. b: If x is greater than b.
map
Description
Re-maps a number from one range to another. That is, a value of fromLow would get mapped to toLow, a value of fromHigh to toHigh, values in-between to values in-between, etc.
Syntax
map(value, fromLow, fromHigh, toLow, toHigh)
Parameters
value: The number to map
fromLow: The lower bound of the value's current range
fromHigh: The upper bound of the value's current range
toLow: The lower bound of the value's target range
toHigh: The upper bound of the value's target rangeReturns
The mapped value.
pow
Description
Calculates the value of a number raised to a power.
Syntax
pow(base, exponent)
Parameters
base: The number (float)
exponent: The power to which the base is raised (float)Returns
The result of the exponentiation (double)
sqrt
Description
Calculates the square root of a number.
Syntax
sqrt(x)
Parameters
x: The number, any data type
Returns
Double, the number's square root.
Example
Output a calculation with constrain() and pow().
#include <Arduino.h>
void setup(){
Serial.begin(9600);
}
void loop(){
Serial.println("Calculate the area of a circle ");
Serial.println("Input value 0-9");
while(!Serial.available());
int d = Serial.read();
d = constrain(d - 0x30, 0, 9); //convert from ASCII to numeric, and remove error value
Serial.print(d);
Serial.print(" x ");
Serial.print(d);
Serial.print(" x 3.14 = ");
Serial.println(pow(d, 2) * PI);
}