Description
Returns the file list in a specified folder.
CAll (METHOD = GET)
http://tool-cloud2.renesas.com/system/api/?key=[API_KEY]
&module=structure&action=list&project=[PROJECT_NAME]
&path=[FOLDER_PATH]
PROJECT_NAME: Specify PROJECT_NAME obtained as project information.
FOLDER_PATH: Specify FOLDER_PATH obtained as path information. / indicates root.
Result
{
"structure": [
{
"path": "[OBJECT_PATH]",
"name": "[OBJECT_NAME]",
"type": "[OBJECT_TYPE]"
},
...
]
}
OBJECT_PATH: Indicates object path.
OBJECT_NAME: Indicates file or folder name.
OBJECT_TYPE: 1 in case folder, 2 in case file, null in case no file and folder.