Overview
Description
Topics
The following products are now supported by LLVM compiler. For details, please refer to Tool News.
・[Upgrade to Revision]RL78 Family Renesas Flash Driver RL78 Type 01 SC Version V1.20 (PDF | English, 日本語)
The following products are now supported by LLVM compiler. For details, please refer to Tool News.
・[Upgrade to Revision]RL78 Family Renesas Flash Driver RL78 Type 01 SC Version V1.20 (PDF | English, 日本語)
The code flash library is free-of-charge software that reprograms the contents of the code flash memory by user programs.
"Renesas Flash Driver for RL78" is free-of-charge software that reprograms the contents of code flash memory and data flash memory by user programs.
Features
- Flash Self Programming Libraries provide the interface for operations on the code areas of flash memories that MCUs have. (Functions are supported varies with the MCU. Please check the available functions in the user's manual for the target flash reprogramming software.) :
- Erasing
- Programming
- Internal verification
- Blank checking
- Security settings, etc.
- An EEPROM emulation library for code flash memory is also included.
- Learn More
Release Information
Flash Self Programming Library Type01 for the RL78 Family
- Latest Ver.: Ver.4.00
- Released: Feb 05, 2024
Note: The LLVM compiler version was added to the package.
Renesas Flash Sample Program Type01 for RL78/G15 Group and RL78/G16 Group
- Latest Ver.: Ver.1.20
- Released: Dec 20, 2023
Renesas Flash Driver RL78 Type 01 for RL78/G2x Group
- Latest Ver.: Ver.1.20
- Released: Sep 20, 2023
Renesas Flash Driver RL78 Type 02 for RL78/F23 and RL78/F24
- Latest Ver.: Ver.1.00
- Released: Aug 05, 2022
Details of upgrade (See Tool News)
Target Devices
Design & Development
Videos & Training
How to Use Renesas Flash Driver RL78 Type 01 SC Version on e² studio
This video introduces how to reprogram the RL78/G2x data flash memory using the Renesas Flash Driver RL78 Type 01 Smart Configurator Version on e² studio.
Chapter's Title & Time
00:00 Opening
00:25 Creating a New Project
01:05 Setting for the Smart Configurator
02:10 Setting for build
03:33 Setting for debug
04:05 Debugging for the Sample program
Additional Details
Distribution Method
Target Device Family | Distribution Method | Software name described in the download list |
---|---|---|
V850 | Download | Flash Self Programming Library Note1 |
RL78/x1x | Download | Flash Self Programming Library Note2, 3 Renesas Flash Sample Program Type01 Note4 |
RL78/x2x | Sample Code | Renesas Flash Driver RL78 Type01 Note5 Renesas Flash Driver RL78 Type02 Note6 |
78K (78K0, 78K0R) | Download | Flash self programming library EEPROM emulation library |
RX | Application notes and sample codes for RX family related to flash programming are available. Please visit the Application Notes & Sample Code of the Documentation tab on the RX family product page. | - |
Notes:
- For the EEPROM emulation library, contact your local Renesas Electronics marketing office or distributor.
- In the User's Manual (Hardware) for some RL78 MCUs or the User's Manual for some Flash Libraries for the RL78 family, the self RAM areas used in common for all flash libraries may be shown. However, for the latest information, please refer to the RL78 Family Self RAM list of Flash Self Programming Library Rev.3.05 (PDF | English, 日本語).
- As the self RAM areas are used as the work area for the library, using these areas for the user program is prohibited. For the latest information, please refer to the RL78 Family Self RAM list of Flash Self Programming Library Rev.3.05 (PDF | English, 日本語).
- Renesas Flash Sample Program Type01 for RL78/G15 group and RL78 G16 group can be downloaded from Sample Code.
- Refer to Renesas Flash Driver and EEPROM Emulation Software for RL78 Target MCU List - General-Purpose (PDF | English, 日本語) for Renesas Flash Driver and EEPROM Emulation Software target MCUs for non automotive use.
- Refer to Renesas Flash Driver and EEPROM Emulation Software Target MCU List for RL78 - Automotive (PDF | English, 日本語) for Renesas Flash Driver and EEPROM Emulation Software target MCUs for automotive use.
Target Devices
- V850 Family
- RL78 Family
- 78K Family (78K0 and 78K0R)