Skip to main content
Renesas Electronics Corporation

Overview

Description

Image
Wi-Fi Development Banner

Wi-Fi implementation is made simple and fast by adding a comprehensive suite of AT-Commands to our wireless family (DA16200 Wi-Fi and DA16600 Wi-Fi/Bluetooth® Low Energy combo).

You can access the industry-leading low power features of the DA16200/DA16600 family simply, quickly and without having to develop any complex software on the Wi-Fi side.

  • A full end-to-end solution
  • Fast prototyping, fast implementation, fast to market
  • Ready to use examples for drag and drop
 

Benefits

  • Fast and easy development
  • Limited software development
  • No Wi-Fi stack knowledge needed
  • Fully certified DA16200 module
Image
AT Command

Features

  • Wi-Fi provisioning
  • MQTT commands
  • Sleep commands
  • Firmware update Over-the-Air commands (OTA)
  • GPIO configuration commands
  • Custom AT

Target Devices

Downloads

Documentation

Design & Development

Sample Code

Videos & Training

How to Get Started

Support

Support Communities

  1. Disable clean session when connecting to MQTT broker using AT command (DA16200)

    ... to MQTT broker via AT command in DA16200? Is the clean session flag automatically disabled when we use QoS 1?   some context: I am using DA16200 as a wifi module and communicate with it via AT command. I found a problem when I try to have a persistent session with ...

    Feb 4, 2022
  2. Reproducing the official "WiFi AT Command Set" firmware image

    Hello, I wonder how to reproduce the official AT-CMD firmware image, using the DA16200 FreeRTOS SDK.More specifically, DA16200_FBOOT-GEN01-01-922f1e27d_W25Q32JW.img DA16200_FRTOS-GEN01-01-56c232799-004158.img from this link. Which configuration header files are relevant?Which compilation flags need to be enabled/ ...

    Jul 4, 2023
  3. DA16200 MQTT DPM

    ... is in DPM mode and the device wakes up with "+INIT:WAKEUP,UC " message and then the device goes to sleep suddenly and thereafter no AT commands working. I've followed the instruction on the AT command reference manual "DA16200 AT Command UM-WI-003" "Procedure to Process MQTT Messages".

    Feb 8, 2022
View All Results from Support Communities (214)

Knowledge Base

  1. There are already so many smart home protocols these days. Why should I consider adding Matter?

    ... applications communicate with each other and with the underlying hardware and operating system. Other protocols that are commonly used in smart home systems, such as Wi-Fi, Bluetooth, Zigbee, and Z-Wave, operate at lower layers of the stack and are responsible for managing the physical connection between devices. Matter ...

Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?