Skip to main content

Overview

Description

Topics
[Upgrade to Version] e² studio 2025-01 (PDF | English, 日本語)
Supports Smart configurator for RISC-V MCU V1.3.0.

e² studio is an Eclipse-based integrated development environment (IDE) for Renesas MCUs. In addition to Eclipse’s own powerful code editor, e² studio offers a rich range of extended functions. e² studio covers all development processes, from the downloading of sample code to debugging.

 

Release Information

Target Devices

Downloads

Type Title Date
Upgrade - IDE Log in to Download ZIP 1,652.42 MB 日本語
Upgrade - IDE Log in to Download RUN 1,528.26 MB 日本語
2 items

Documentation

Design & Development

Videos & Training

e² studio Tips: How to Use the Expressions View During Debugging

The Expressions view in e² studio lets you monitor the values of variables and expressions during debugging, among other features. This video demonstrates how to use the Expressions view.

Related Resources

Video List

Additional Details

e² studio

See the table below for features of the software and tools available for use with the e² studio on RISC-V MCU products.
For an overview of the functions and features of the e² studio, refer to e² studio (the general page).

Code generation support and other useful functions for RISC-V MCUs

Tool nameDescription
Smart ConfiguratorA GUI-based tool that provides support for downloading and importing middleware for code generation and configuring various settings
Smart BrowserA function that allows you to easily search and show the latest version of the hardware manual, technical updates, application notes, and tool news for the Renesas microcontroller you are using

Compilers for RISC-V MCUs

Supported CompilerInformation on usage
Open Source
・LLVM for Renesas RISC-V MCU
  • The GNU compilers can be installed through selection with the installer of the e² studio. This requires an Internet connection.
  • The GNU compilers can be installed free of charge by downloading from the GNU Web site (https://llvm-gcc-renesas.com).
    Registration of these compilers with an e² studio which has already been installed is required.
  • LLVM for Renesas RISC-V MCU is available for 2024-01.1 and later versions of the e² studio.

 

Debugging tools for RISC-V MCU

Note

  • Product from a Renesas partner