Skip to main content

PG-FP5 Information for Users

PG-FP5

PG-FP5 How to Find the Version Number

Programming GUI, Firmware and FPGA for PG-FP5

To check the version number, follow these steps:

Step1. PG-FP5 Startup

After the cables are connected, press the POWER button on the PG-FP5.

Step2. Startup of Programming GUI

Click the Start menu, "All Programs", point to "Renesas Electronics Utilities", "Programming Tools", and then select "PG-FP5 Vx.xx" of "PG-FP5 Vx.xx" to start the Programming GUI. When communication is established and the programming GUI is correctly started, the main window will be opened.

Step3. Check the Version Numbers of the Programming GUI, Firmware and FPGA with "Reset Command" or "Main Window", as Shown Below:

  • Programming GUI
    • - Open the Help menu and click the About FP5 command.
    • The version number of Programming GUI is displayed in the About FP5 dialog box.
    • or
    • - Refer to the programming parameter window on the right of the main window. The version number of Programming GUI is shown at the FP5_GUI row in the Programmer box of the programming parameter window.
  • Firmware
    • - Open the Programmer menu and click the Reset command.
    • The version number of Firmware is displayed in the action log window.
    • or
    • - Refer to the programming parameter window on the right of the main window. The version number of Firmware is shown at the Firmware row in the Programmer box of the programming parameter window.
  • FPGA
    • - Open the Programmer menu and click the Reset command. The version number of FPGA is displayed in the action log window.
Image

Display Example of Reset Command

Image

Display Example of Main Window