Skip to main content

Firmware Integration Technology (FIT)

RX Driver Package

FIT Information

Firmware Integration Technology (FIT) simplifies embedding peripheral function module drivers and allows portability between RX microcontrollers, with the aim of reducing the burden of program development and software resource management in software development using the RX Family.

About FIT

Features of FIT

FIT lays out clear rules for sample code (middleware and drivers) provided for RX Family devices as follows.

  • MCU initial settings
  • How to define a target board
  • File configuration
  • Names of functions
  • Common interface with user application

Conventionally, the above information has in many cases varied by sample code, so changes needed to be made to sample code when embedding into a user application. With FIT, there are rules for this information, so each sample code can be embedded into a user application with ease. Also, the peripheral function drivers and middleware which support FIT have a common interface with user applications. This makes it easy to port user applications when migrating between RX microcontrollers.

FIT modules emphasize portability between RX family microcontrollers.

FIT modules emphasize portability between RX family microcontrollers.

Easy Embedding to Project Generated by Integrated Development Environment

The e2 studio integrated development environment (IDE) which is based on the globally popular Eclipse open source IDE has a GUI (plug-in feature) for embedding FIT modules. Using this feature, FIT modules can be embedded with ease into projects generated in e2 studio. FIT modules also support CS+.

Configuration of FIT

FIT consists of a Board Support Package (BSP), peripheral function modules, and middleware modules.

  • BSP
    Module that performs initial MCU settings, clock settings, board settings, and so on
  • Peripheral Function Modules
    Drivers that control the peripheral functions of a RX microcontroller
  • Middleware Modules
    Middleware function such as TCP/IP and file system

Using FIT modules helps ease development.

Using FIT modules helps ease development.

Advantages of FIT

1. Embed Peripheral Function Modules With Ease

Drivers and Middleware Supporting FIT

Peripheral function modules and middleware modules that support FIT operate in a common MCU basic setting (BSP).

Peripheral function modules and middleware modules that support FIT operate in a common MCU basic setting (BSP).

Conventional Drivers and Middleware

Conventional Drivers and Middleware

2. Migrate Between RX Microcontrollers With Ease

Drivers and Middleware Supporting FIT

Once FIT is supported, the APIs of peripheral driver modules and middleware modules have common specifications. The MCU can be switched easily to another MCU.

Drivers and Middleware Suppoting FIT

Conventional Driver and Middleware

Sample code and middleware which do not support FIT do not have a common API. Migrating between products takes many man-hours.

Conventional Driver and Middleware

Obtaining the Product

Peripheral function modules and middleware modules that support FIT are included with the RX Driver Package. Please download the RX Driver Package.
You can confirm the device support status of each Firmware Integration Technology module included in the latest version of the RX Driver Package by viewing the List of FIT Modules ( XLSX version or PDF version ).

Implementing FIT

Please refer to the following before implementing FIT modules. We recommend using the Smart Configurator.

User's Manual

RX Smart Configurator User' Guide

Application Note

Application Sample Code